---
title: "Automated Design Checker"
slug: "automated-design-checker"
updated: 2025-06-26T19:01:00Z
published: 2025-06-26T19:01:00Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Automated Design Checker

Learn how to use MachineBuilder’s Automated Design Checker to validate and improve your Vention assembly by detecting and resolving key design issues.

## **Feature Overview**

The Automated Design Checker is a smart tool that scans your assembly to identify and assist in resolving design issues. It checks for potential errors such as:

- Missing End Caps
- Missing Plates or Frame Connectors
- Proper Usage of Profiles
- Unformed Connections
- Floating Components
- Interfering Components
- Missing Panel Holes
- Missing Automation Components
- Obsolete or Deprecated Components
- Hidden Components

## **Using the Automated Design Checker**

1. Select **Automated Design Check** from the Navigation Bar. The tool will scan your design and display any detected issues in a notification window.
2. Expand any section to view the list of identified issues.
3. Click an error name to snap the camera to the issue and highlight the relevant components.
4. Resolve the issues using one of the following methods:
  - **Add Component:** If an **Add** button appears, click it to automatically fix the issue by adding the necessary component.
  - **Dismiss:** Click the **Dismiss** button to remove the error from the list without making changes.
  - **Manual Fix:** Modify your design directly to correct the problem.

Once all necessary changes are made, close the **Automated Design Check** window.