---
title: "Custom HMI Development"
slug: "custom-hmi-development"
updated: 2026-04-01T12:56:14Z
published: 2026-04-01T12:56:14Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Custom HMI Development

We now provide a starter template with all the code necessary to run, display, and automatically rebuild a React application when changes are detected.

### Quick Start - Hello World Example

The simplest possible UI application consists of an `index.html` file in the `ui/` folder with plain HTML, CSS, and JavaScript — no build step required.

1- Inside a new Python application, create a new directory and give it the name `ui`

2- In the new `ui` directory, create a new file and name it `index.html`

3- open the `index.html` file and paste this snippet:

```xml
<!doctype html>
<html lang="en">
  <head>
    <meta charset="UTF-8" />
    <meta name="viewport" content="width=device-width, initial-scale=1.0" />
    <title>My HMI</title>
    <style>
          button { font-size: 100px }
    </style>
  </head>
  <body>
    <div id="root">
      
      <button id="mybutton" onclick="ThisIsAButton()">
        This is a Button! 
      </button>
    </div>
    <script>
      function ThisIsAButton() {
        alert("Hello World!")
      }
    </script>
  </body>
</html>
```

4- to see the Custom UI in action, select the **Open HMI** button. you will see the content of the `index.html` rendered in our HMI visualizer:

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(580).png)

Simple Custom HMI example

## Getting Started

### Option 1: Using the Application Template (Recommended)

Simply select **PythonTemplate** in the Machine Logic **New Application** dropdown. This will provide you with everything you need to start developing your custom UI application.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/application template.png)

Accessing the application template

---

### Option 2: Local Development Setup

If you decide to start your frontend application locally instead, you'll need to ensure your project configuration matches the required specifications.

#### Step 1: Configure package.json

Your `package.json` must have versions that match the demo, in particular for **Vite** and **React**:

```json
{
  "name": "your-custom-ui-app",
  "version": "1.0.0",
  "type": "module",
  "scripts": {
    "dev": "vite",
    "build": "vite build",
    "preview": "vite preview"
  },
  "dependencies": {
    "@emotion/react": "11.13.3",
    "@emotion/styled": "11.13.0",
    "@mui/icons-material": "5.16.7",
    "@mui/material": "5.16.7",
    "@mui/styles": "5.16.7",
    "@tabler/icons-react": "3.35.0",
    "@vention/machine-logic-ui-sdk": "0.27.3",
    "@vention/machine-ui": "3.38.0",
    "@vention/machine-apps-components": "0.3.22",
    "buffer": "6.0.3",
    "dayjs": "1.11.18",
    "react": "17.0.2",
    "react-dom": "17.0.2",
    "react-draggable": "4.4.6",
    "react-hook-form": "7.53.0",
    "react-router-dom": "6.26.2",
    "tss-react": "4.9.13"
  },
  "devDependencies": {
    "@types/node": "^20.10.0",
    "@types/react": "17.0.82",
    "@types/react-dom": "17.0.25",
    "@vitejs/plugin-react": "^4.3.4",
    "typescript": "5.4.5",
    "vite": "^6.0.0"
  },
  "engines": {
    "node": ">=20",
    "npm": ">=8"
  }
}
```

**Critical versions to match:**

- React: `17.0.2`
- Vite: `^6.0.0`
- TypeScript: `5.4.5`

#### Step 2: Configure vite.config.ts

Create a `vite.config.ts` with the following configuration:

```typescript
import { defineConfig } from "vite"
import react from "@vitejs/plugin-react"
import path from "path"
export default defineConfig({
  plugins: [react()],
  base: "./",
  resolve: {
    alias: {
      "@": path.resolve(__dirname, "./src"),
    },
  },
  build: {
    outDir: "../ui",
    emptyOutDir: true,
    minify: "esbuild",
    target: "esnext",
    cssMinify: "esbuild",
    sourcemap: false,
  },
  server: {
    port: 5173,
    host: true,
    hmr: {
      overlay: true,
    },
  },
  optimizeDeps: {
    include: ["react", "react-dom", "@mui/material", "@emotion/react", "@emotion/styled"],
  },
})
```

**Key configuration points:**

- `base: "./"` - Uses relative paths for assets (required for proper loading)
- `outDir: "../ui"` - Outputs build to the `ui` folder at the parent level
- `target: "esnext"` - Modern JavaScript output

---

## Autobuild Feature Requirements

To enable the automatic rebuild feature, your project must follow this folder structure:

### Required Folder Structure

```plaintext
your-application/
├── customui/          ← Your react source code goes here
│   ├── src/
│   │   └── main.tsx
│   ├── index.html
│   ├── package.json
│   ├── vite.config.ts
│   └── tsconfig.json
└── ui/                ← Build output goes here (auto-generated)
    ├── index.html
    └── assets/
        ├── main.js
        └── main.css
```

### Build Output Requirements

Your build script must output the built files to a `ui` folder at the **same level** as the `customui` folder. With the `vite.config.ts` provided above, running `vite build` will automatically output to `../ui`, which satisfies this requirement.

---

## Summary

| Requirement | Details |
| --- | --- |
| Source folder | `customui/` |
| Build output folder | `ui/` (same level as customui) |
| React version | 17.0.2 |
| Vite version | ^6.0.0 |
| Node.js | >=20 |
| npm | >=8 |
| Build base path | `"./"` (relative) |
| Target | `esnext` |

For the quickest setup, use the **Application Template** option in Machine Logic. For custom local development, ensure all configurations match the specifications above.

---

## Advanced: Faster Build with esbuild

The Application Template includes an optimized build script using esbuild directly, which is faster than the standard Vite build. If you want to use this approach, update your `package.json` with the following:

```json
{
  "scripts": {
    "dev": "vite",
    "build": "esbuild src/main.tsx --bundle --outdir=../ui/assets --format=esm --target=esnext --loader:.tsx=tsx --loader:.ts=ts --loader:.css=css --splitting --entry-names=main --chunk-names=[name]-[hash] && sed 's|/src/main.tsx|./assets/main.js|g' index.html | sed 's|</head>|<link rel=\"stylesheet\" href=\"./assets/main.css\"></head>|g' > ../ui/index.html && chmod -R g+w ../ui",
    "preview": "vite preview"
  },
  "devDependencies": {
    "esbuild": "^0.24.0"
  }
}
```

### Build Script Breakdown

This script performs the following steps:

```bash
# 1. Bundle with esbuild
esbuild src/main.tsx --bundle --outdir=../ui/assets \
  --format=esm --target=esnext \
  --loader:.tsx=tsx --loader:.ts=ts --loader:.css=css \
  --splitting --entry-names=main --chunk-names=[name]-[hash]
# 2. Transform index.html and output to ui folder
sed 's|/src/main.tsx|./assets/main.js|g' index.html | \
sed 's|</head>|<link rel="stylesheet" href="./assets/main.css"></head>|g' \
> ../ui/index.html
# 3. Set group write permissions
chmod -R g+w ../ui
```

**What each part does:**

1. **esbuild bundling** - Compiles and bundles the TypeScript/React code with code splitting enabled
2. **HTML transformation** - Updates `index.html` to reference the built assets:
  - Replaces `/src/main.tsx` with `./assets/main.js`
  - Adds the CSS stylesheet link to the head
3. **Permissions** - Sets group write permissions on the output folder

This approach is faster for incremental rebuilds but requires the additional `sed` commands to transform the HTML file.