---
title: "Datalogic Laser Scanner & Light Curtain User Manual"
slug: "datalogic-laser-scanner-light-curtain-user-manual"
updated: 2026-01-08T18:15:46Z
published: 2026-01-08T18:15:46Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Datalogic Laser Scanner & Light Curtain User Manual

## Overview

Safety devices are essential for a safe work environment. They can be used in various configurations to monitor safety zones where access is limited. Four safety devices (laser scanners, light curtains or fail safe proximity sensors) can be connected to Vention’s Muting Safety Module AI at a time. If you need to interface more safety devices to MachineMotion AI, you can add Muting Safety Modules AI (daisy-chained). Please refer to the User Manual of the Muting Safety Module AI for more information about the connections.

> [!WARNING]
> This document covers requirements for the latest version of Datalogic Laser Scanner & Light Curtain. For previous version, refer to link below:
> 
> [*Documentation for Previous Product Versions*](/technicaldocumentation/docs/datalogic-laser-scanner-light-curtain-user-manual#documentation-for-previous-product-versions)

## Laser Scanner (Parent only)

### Description

The Datalogic Laser Scanner (PR-DA-001-0489) is an essential tool to ensure safety in the workplace. It can be used in multiple orientations to monitor large areas while remaining discreet and unobstructive. It will stop a machine if any undesired person or object crosses its safety zone. A PC with an Ethernet port is required for configuration. In order to use the Laser Scanner with MachineMotion AI, a Muting Safety Module (CE-SA-015-0001__2) is required, please refer to the safety installation guideline section for the wiring. The Laser Scanner specifications are as follows:

- Maximum safe zone: 5.5 m radius.
- Maximum warning zone: 40 m radius.
- Detection angle: 275o.
- Total/partial dynamic muting available.
- Zone switching (bank switching) available.
- 12-pin M12 connector available for communication with Muting Safety Module (CE-SA-015-0001__2).
- 4-pin M12 connector available for programming and monitoring (via an Ethernet cable to a computer).

### Getting Started

1. Assemble the Laser Scanner bracket and mount it at the desired location.

| ![Figure 1: Laser Scanner bracket](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/bracket-exploded-view.png) ***Figure 1: Laser Scanner bracket*** |
| --- |
2. Download the latest version of the DL Sentinel software from [here](https://www.datasensing.com/eng/downloads-dw-82.html).
3. Connect scanner to PC with the provided programming cable.
4. On the PC, open the DLSentinel software, and navigate to Scanner > Discovery. Your scanner should appear on the left panel. Select your scanner. A warning window may appear asking to change your IP address. Select OK.

| ![Figure 2: Warning](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/06978f89-0d2f-4f2d-82c3-10a502203406) ***Figure 2: Warning*** |
| --- |
5. Align the IP address. To align the IP address, make sure DHCP is set to Static. Verify that the last number of the IP Local address is different from the last number of the IP address. In figure 3, the last digits are 122 and 71, which are different.

| ![Figure 3: IP and IP Local Addresses](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/f9807601-0c7c-4e8b-973b-6c3c3f08b43b) ***Figure 3: IP and IP Local Addresses*** |
| --- |
6. On the main screen of the DLSentinel software, select Open a Safety System configuration from PC. Open the initialization file and select the connected laser scanner from the panel on the left side of the screen

### Parameters’ configuration

Perform the following steps to get access to the Configuration settings:

- Open the connected scanner in the DLSentinel software by navigating to Scanner > Discovery. The connected scanner will be visible in the left-hand column
- Select your scanner and click on the white arrow at the top-right corner of the screen

To set parameters, select Configuration to access a drop-down menu. For each item on the drop-down menu, enter the desired values in the appropriate fields (highlighted in yellow). More details are provided for each parameter below.

| ![Figure 4: Configuration settings page](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/03ab5305-e56f-4f00-8494-724f9eb8a40d) ***Figure 4: Configuration settings page*** |
| --- |

1. Outputs:
  1. **Auto Reset** can be set to ENABLED or DISABLED. If the Laser Scanner boots with an error (such as both zones are activated, or no zones are activated), this function will automatically restart the Laser Scanner after 10 seconds. However, if the device locks in INTFx more than five times within 15 minutes (see Datalogic documentation for more details), Auto Reset will not activate, and a power cycle will be required to reactivate the device. It is recommended to set Auto Reset to ENABLED to avoid booting errors.

| ![Figure 5: Output configuration](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/d9f8b847-34dc-438a-a50c-115f8ea12234) ***Figure 5: Output configuration*** |
| --- |
2. Zone Set:
  1. **Zone Set No.** can be set to 1 or 2. Use two zones when independent muting of different areas is required (such as for a palletizer with two zones). When setting two zones, click the “01010” icon to automatically fill the area switch pin association.

For a two-zone configuration, 1 1 and 0 0 are invalid Area Switch combinations. This will result in an error state. To resolve it, provide a signal to either Area Switch 1 or Area Switch 2 (effectively creating a 1 0 or 0 1 combination) and restart the Area Scanner.

| ![Figure 6: Zone set configuration](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/29696b08-3510-464e-b8ae-b42ebcbbdcfb) ***Figure 6: Zone set configuration*** |
| --- |
    - Zone Set 1 active when Area Switch 1 = 1 and Area Switch 2 = 0
    - Zone Set 2 active when Area Switch 1 = 0 and Area Switch 2 = 1
3. Inputs:
  1. **Recovery time [msec]** is the time delay between the object leaving the protected area and the OSSDs achieving the NORMAL OPERATION state. The minimum (default) value is 200 ms. It is recommended to keep the default value.

| ![Figure 7: Input configuration](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/061566f7-3103-4cc5-bbbf-67916ce35716) ***Figure 7: Input configuration*** |
| --- |
4. Detection
  1. **Number of scans** controls the number of scans required to validate a detection. This parameter has a direct impact on Response time (more scans results in a longer response time).
  2. **Detection capability [mm]** is the ability to detect an object of given dimensions within the detection zone. Objects greater than or equal to the selected value can be detected in both the safety and warning zones.
  3. **Dust Filter Level** can be set to LOW, MID, or HIGH depending on the environment and the levels of airborne particles.Dust Filter Level should be set to the lowest value that still allows the Laser Scanner to work without detections due to dust.

| ![Figure 9: Detection configuration](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/da27ba4d-5ad8-4c35-b749-7859923cfee5) ***Figure 9: Detection configuration*** |
| --- |
5. Zones
  1. Select the appropriate zone (Zone 1 or Zone 2, if there are two zones) in which to create the safety, warning and muting zones.
  2. To create a warning zone, click **Warning 1**, select a drawing tool from the right side of the screen (freehand, line, circle, arc, or polygon) and draw the desired warning zone. Multiple areas can be defined. The defined warning zones will appear yellow.
  3. To create a safety zone, click **Safety 1**, and repeat the same procedure as above for warning zones. Safety zones will appear red.
  4. To create a reference point, select the 6th icon down from the top right icons and place the point on a surface (such as a door frame or wall). Then set the tolerance. If the reference point moves outside the permitted tolerance, the OSSD will switch to an OFF state.
  5. **NOTE:** According to safety guidelines, when a laser scanner is monitoring a vertical plane, the safety zone should have a maximum gap of 180 mm from the bottom and a minimum height of 1400 mm when there are no height restrictions.

| ![Figure 10: Safety Zones](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/2f02f3c0-6fc9-4789-b926-403b42e46a08) ***Figure 10: Safety Zones*** |
| --- |
  6. Once satisfied with the configuration, click the **Next** white arrow in the top-right corner of the screen. Then click **Load** to upload the configuration to the area scanner. If prompted to enter a password, the default password is “admin” (this can be changed later). A warning will appear saying “Scanner status change in Off-Duty, continue?”. Select OK. Once the configuration is uploaded, click **Accept** to finalize the process.
  7. To ensure everything is working as expected, click **Monitoring** while plugged into the scanner to see a live feed of the scanner functioning. For more information on various display icons that may appear on the Laser Scanner screen, refer to Datalogic’s Quick Guide for the SLS-M5-0812-E model.

## Laser Scanner (Parent & Child Cluster)

### Child Laser Scanner Description

The usage of Child Laser Scanners (PR-DA-001-0582) in combination with Parent Laser Scanners should be considered when the user wants to monitor multiple planes and/or areas that may be obstructed or not visible by a single Parent Laser Scanner. The Child Laser Scanner specifications are as follows:

- Maximum safe zone: 5.5m radius.
- Maximum warning zone: 40m radius.
- Detection angle: 275o.
- Total/partial dynamic muting available.
- Zone switching (bank switching) available.
- Daisy-chain cable included.
- The maximum number of units in a cluster is 4, consisting of 1 Parent Scanner and 3 Child Scanners.

### How to Configure a Parent-Child Cluster

To configure a laser scanner cluster comprised of a Parent Scanner and up to three Child Scanners, perform the following steps:

1. Connect the scanners as illustrated below using the included daisy-chain cables.

| ![image](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/parent-child-daisy-chain-diagram.png) |
| --- |
2. Follow steps 2 to 6 of the *Getting started* section for the Parent scanner.
3. Select the Parent Scanner on the left side of the DLSentinel window and click the white arrow at the top-right corner of the screen.
4. Configure the Parent Scanner using the Configuration drop-down menu located in the top-left corner of the screen. See the Parameters’ configuration section of the Parent Scanner for more information.
5. Select a Child Scanner on the left side of the DLSentinel window and click the white arrow at the top-right corner of the screen.
6. Under the Configuration drop-down menu, only configure the Detection and Zones items.
7. Repeat steps 5 and 6 for each Child Scanner in the cluster.
8. Once satisfied with the configuration, click the **Next** white arrow in the top-right corner of the screen. Then click **Load** to upload the configuration to the area scanner cluster. If prompted to enter a password, the default password is “admin” (this can be changed later). A warning will appear saying “Scanner status change in Off-Duty, continue?”. Select OK. Once the configuration is uploaded, click **Accept** to finalize the process.
9. To ensure everything is working as expected, click **Monitoring** while plugged into the scanner to see a live feed of the scanners functioning.

For more information on various display icons that may appear on the Laser Scanner screen, refer to Datalogic’s Quick Guide for the SLS-M5-0812-E (Parent Scanner) & SLS-R5-E (Child Scanner) models.

### Troubleshooting

If the parent and the child scanners are not able to communicate to each other or cannot be configured together, make sure that they are all on the same firmware version.

If a child scanner is disconnected or missing from the cluster that has been programmed and uploaded, the parent scanner will fall into an endless power cycle loop. To solve this, either reconnect the missing scanner(s) or disconnect all children scanners and upload a parent-only configuration to the parent scanner (follow steps 2 to 6 in *Getting started* for the parent scanner) to regain access to the parent scanner. Then, reconnect the children scanners to the cluster and reconfigure the cluster as desired.

## Light Curtain

### Description

The Datalogic Light Curtain (PR-DA-001-0295 & PR-DA-001-0296) is a useful device to increase safety in various industrial applications. It is generally used to monitor and control the entry and/or exit of objects across a safety barrier. If an unwanted object or person crosses the safety barrier, the Light Curtain will stop the machine it is connected to. In order to use the Light Curtain with MachineMotion AI, a Muting Safety Module (CE-SA-015-0001__2) is required, please refer to the installation instructions below.

The Light Curtain specifications are as follows:

- Resolution type: 4 (finger and hand protection).
- Resolution: 30 mm.
- Monitored height: 750 mm.
- Maximum operating distance: 20 m.
- Muting available.

### Getting Started

1. Choose an appropriate position for the light curtain, and mount both the emitter and the receiver with the connectors pointing in the same direction using the included mounting brackets.
2. The light curtain should be carefully positioned to provide the necessary protection. Access to the dangerous area must only be possible by passing through the light curtain safety zone

### Configuration - Disabling External Device Monitoring (EDM) for Rx Light Curtain Only

Before connecting the Light Curtain to the Muting Safety Module AI and MachineMotion AI, make sure it is in the basic configuration. Follow the steps below to configure the Light Curtain.

**Note:** Use the associated tool tip provided to press the buttons.

1. Keep the CONFIRM button pressed for 5 seconds to enter Basic Configuration Mode.
2. A Test Pattern is shown on led interface; carefully check that ALL LED are lit in sequence from 2 to 8, then current configuration is shown.

| ![Figure 11: Test Pattern LED Status](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/c5f45c28-2730-47e4-a49c-f93364c88dce) ***Figure 11: Test Pattern LED Status*** |
| --- |
3. Press SELECT until the ACM LED is BLINKING.
4. Press ENABLE until the ACM LED is OFF.
5. Press CONFIRM for 5 seconds to authorize the new configuration. The LEDs on the light curtain should now be displayed as below.

| ![Figure 12: Final LED Status](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/df1f6837-b94f-4690-a028-eb1cca38970c) ***Figure 12: Final LED Status*** |
| --- |

## Safety Installation guidelines

Light curtains or laser scanners must be installed in compliance with the standard ISO 13855 - 2024, Safety of machinery — Positioning of safeguards with respect to the approach of the human body and a risk assessment must be performed to unsure suitability to the application.

## Connecting to MachineMotion AI

### Laser Scanner

The steps to connect the Laser Scanner to MachineMotion AI via the Muting Safety Module AI are as follows:

1. Connect the Laser Scanner to a Muting Safety Module (CE-SA-015-0001__2) to one of the DEVICE connectors using the Area Scanner Cable (CE-SA-104-0001)*.
2. Connect a MachineMotion AI Safety Extension Cable (CE-CA-102-5000__3) to the Muting Safety Module AI’s SAFETY OUT connector and MachineMotion AI’s SAFETY IN connector.
3. If muting is required, connect the muting sensor of the muting kit (CE-AP-002-0000__2) in pairs thanks to the Muting Sensor Y Adapter (CE-SA-107-0001). Then connect the adapter to the Muting Safety Module AI via the MUTING xA and MUTING xB connectors.

*If a cluster of Parent-Child Scanners are being used, make sure to make all daisy-chain connections prior to connecting to MachineMotion AI.

**Note:** If no other safety modules are being daisy-chained to the Muting Safety Module AI, a safety jumper (CE-SA-102-0001) must be used on the Muting Safety Module AI’s SAFETY IN connector. Safety Device Jumper (CE-SA-125-0001) must be connected to the unused DEVICE connectors.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with Muting and Datalogic Area Scanner.png) ***Figure 13: Laser Scanner (Parent only) wiring diagram*** |
| --- |

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with Muting and Datalogic Area Scanner daisychained.png) ***Figure 14: Laser Scanner (Parent-Child cluster) wiring diagram*** |
| --- |

### Light Curtain

The steps to connect the Light Curtain to MachineMotion AI via the Muting Safety Module AI are as follows:

1. Connect the receiver and the emitter to CE-SA-106-0001 cable. Then, connect CE-SA-106-0001 to one of the Muting Safety Module AI’s DEVICE connectors.
2. Connect a MachineMotion AI Safety Extension Cable (CE-CA-102-5000__3) to the Muting Safety Module’s SAFETY OUT connector and MachineMotion AI’s SAFETY IN connector.
3. If muting is required, connect the muting sensor of the muting kit (CE-AP-002-0000__2) in pairs thanks to the Muting Sensor Y Adapter (CE-SA-107-0001). Then connect the adapter to the Muting Safety Module AI via the MUTING xA and MUTING xB connectors.

**Note:**If no other safety modules are being daisy-chained to the Muting Safety Module AI, a safety jumper (CE-SA-102-0001) must be used on the Muting Safety Module AI’s SAFETY IN connector. Safety Device Jumper (CE-SA-125-0001) must be connected to the unused DEVICE connectors.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with Muting and Datalogic Light Curtains.png) ***Figure 15 Light curtain wiring diagram*** |
| --- |

## Muting

The muting function automatically deactivates the safety status of the whole safety area (total muting) or part of it (partial muting). This feature is particularly suitable when an object, but not a person, has to pass through the dangerous area. This feature also allows carrying out cyclical operations without blocking a working machine.

Muting sensors must be placed according to the material’s length and speed so they can recognize passing objects (such as pallets, vehicles, etc). When using the Muting Safety Module AI, four muting sensors are required to perform a bidirectional muting.

**Bidirectional muting** is used for objects entering and leaving an area. In this case, four sensors must be used: two on one side of the safe zone (A1 and B1), and two on the other side (A2 and B2). Sensors A1 and A2 are connected together, and B1 and B2 are connected together. They should be spaced at a distance where two consecutive sensors are always triggered throughout the movement of the object across the safety zone.

| ![Figure 17: Bidirectional muting](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/bidirectional-muting-diagram(1).png) ***Figure 17: Bidirectional muting*** |
| --- |

### Documentation for Previous Product Versions

****Keyence Laser Scanner & Light Curtain User Manual****

[Datalogic Laser Scanner & Light Curtain User Manual](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Datalogic%20Laser%20Scanner%20%20Light%20Curtain%20User%20Manual.pdf)