---
title: "Get Started: RemoteView for MachineMotion V2"
slug: "get-started-remoteview"
updated: 2025-05-06T02:55:40Z
published: 2025-05-06T02:55:40Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Get Started: RemoteView for MachineMotion V2

## **Prerequisites**

In order to get access to RemoteView, you will need the [Remote Camera Kit](https://vention.io/parts/remote-camera-kit-2501) and a [valid subscription](https://vention.io/subscriptions).

## **Technical Specifications**

Technical Specifications for the [Remote Camera Kit](https://vention.io/parts/remote-camera-kit-2501) :

| Vertical adjustment range | 120 mm |
| --- | --- |
| Horizontal adjustment range | 90 mm |
| Angular adjustment range | +/- 45 degrees |

## **Getting Started**

### Assemble & Adjust Hardware

1. Mount the articulated arm to your structure using the two included M8 x 16mm screws and a 5mm hex drive. **Note**: For best camera quality and mechanical reliability, mount the articulated arm on a part of your structure where vibrations are minimal.
2. Adjust the camera position by using the adjustment screw on the [Round to Round Angle Connector](https://vention.io/parts/round-to-round-angle-connector-1093) as shown below. This allows you to precisely aim the camera at your desired area.

| ![Articulated Arm Adjustability](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/remote-view-camera-new.png) ***Articulated Arm Adjustability*** |
| --- |

### Connect your camera

The camera cable has a nominal length of 5 meters and comes already pre-mated to the remote viewing camera. Simply connect the camera cable directly to the MachineMotion on the “Live Camera” port (M12 X coded). If you need to extend the camera cable, you can:

1. Unmate the camera and the camera cable,
2. Insert a standard M12 A-coded 8-position male-female cable (such as [CE-CA-022-5000](https://vention.io/parts/machinemotion-control-device-extension-cable-5m-634)) in-line between the camera and the camera cable.

### Connect to Internet

To establish the connection from your machine to the cloud, you will need to be connected to the internet.

1. In the Control Center, navigate to the **Settings** page
2. From the **Network** section, select and connect to the network of your choice, for example via the Wi-Fi interface.

### Connect to MachineAnalytics

1. Log into your account on the [vention.io](https://vention.io/) platform
2. Navigate to your dashboard and click on the **Analytics** tab

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Analytics20Tab.png) |
| --- |
3. Identify the machine you want to monitor and click on **RemoteView** **Note:** From the moment you connect the camera, allow a few minutes for the camera to be detected and streamed

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Fleet20Dashboard20-20Remote20View.png) |
| --- |
4. Once on the RemoteView page, you should see the live video stream of the camera you just installed **Note:** If you see the “offline” screen, make sure your camera is well connected and that you have an internet connection. Once that is confirmed, refresh the page

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/RemoteView20Stream.png) |
| --- |
5. You can leverage this live stream to move the camera in the desired position for monitoring