---
title: "AC Motor and VFD for Material Handling"
slug: "machinemotion-ai-ac-motor-and-vfd-for-material-handling"
updated: 2025-05-15T19:32:50Z
published: 2025-05-15T19:32:50Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# AC Motor and VFD for Material Handling

> [!WARNING]
> This document covers requirements for current version of MachineMotion controller. For previous version, refer to link below:
> 
> [*Documentation for Previous Product Versions*](/technicaldocumentation/docs/machinemotion-ai-ac-motor-and-vfd-for-material-handling#documentation-for-previous-product-versions)

**Tech specs: Motor and VFD**

| Specification | Value |
| --- | --- |
| Compatible conveyor mounts | MO-CV-003-0001, MO-CV-009-0001, MO-CV-016-XXXX |
| Max power | 1/2 HP (0.37kW) |
| Motor speed range | 431.25 RPM @ 15 Hz to 1725 RPM @ 60Hz |
| Motor output torque | 5.5 Nm* |
| Gearbox reduction ratio options | 3:1, 8:1, 10:1, 15:1 |
| Max conveyor speed | HD: 1200, O-ring: 1500, Belt: 700 (mm/s) |
| Motor input voltage | 230 V |
| Motor cooling method | Air-cooled with fan |
| Gearbox input flange | NEMA 56-C |
| Gearbox output flange | NEMA 34 |
| VFD input voltage | 120 V (North America), 240 V (Europe) |
| VFD IP rating | IP31 |
| Control type | Manual / MachineMotion |
| Combined weight | 12.5 kg |
| Certifications | **Motor**: CE, CSA; **VFD**: CE, UL, CSA, EAC, RoHS2, IE2 |

*Measured at motor breakdown torque

## Safety

Important: Take the following safety precautions when doing any maintenance:

1. Never work on energized equipment.
2. **Always establish the motor connection first before energizing the VFD.**
3. Routinely inspect the motor and gearbox to ensure all bolts are tightened properly.

## Mounting the motor

The motor-gearbox combination come pre-assembled.

To mount the motor:

1. Rotate the conveyor rollers, by hand, to align the drive input keyway with the gearbox output shaft’s orientation.
2. **Apply a small amount of grease to the gearbox output shaft so that it is lightly coated. This will reduce the possibility of fretting corrosion occurring during operation, making future removal easier.**
3. M6 fasteners are provided to attach the gearbox to the conveyor drive input. Ensure the bolts are tightened adequately.
4. M8 hex head bolts ([HW-FN-103-0025](https://vention.io/parts/m8-x-25-mm-hex-head-screw-2523)), T-nuts ([HW-FN-002-0001](https://vention.io/parts/m8-drop-in-spring-loaded-t-nut-265)), washers ([HW-WS-001-0001](https://vention.io/parts/m8-washer-with-16mm-outside-diameter-269)) and split washers ([HW-WS-001-0003](https://vention.io/parts/m8-split-lock-washer-with-127-mm-outside-diameter-2522)) are provided to support the motor mounts. This is recommended as the motor and gearbox will induce a substantial bending moment on the motor mount due to its length and mass. It must also be noted that hole pattern of the base mount does not respect Vention’s 45 mm increment standards.

Some important design considerations:

1. The motor mount support must be designed in away to allow for belt tensioning, such as is required with the HD roller conveyor. For that, it is recommended to use two vertical extrusions as seen below, whereby the M8 fasteners can be loosened, tension adjusted, and then re-secured along that vertical plane.
2. With an appropriate motor mount support designed, ensure that the motor power cable, which is modelled in MachineBuilder, does not intersect with the extrusions. The cable will not be able to sustain very tight bend radii, which may damage it.
3. You don’t need to add 2 extrusions to support the motor mount, even adding 1 extrusion is enough. The pictures below show you some suggested designs for motor mount support designs.

| ![Motor Mounting, Method 1](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/ac-motor-mounting.png) ***Motor Mounting, Method 1*** |
| --- |
| ![Motor Mounting, Method 2](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/ac-motor-mounting-method-2.png) ***Motor Mounting, Method 2*** |

## Mounting the VFD

The VFD supplies the motor with power and controls its speed. MachineMotion can communicate with the VFD and control up to three digital inputs, such as the VFD start-stop function, via the digital IO module.

To mount the VFD:

1. Select the placement area. Choose a dry place, like the side of the structure supporting the conveyor. Leave 150 mm of clearance below the VFD for its electrical cables, and ensure the VFD is within reach of the 2.5 m-long motor power cable.
2. Attach the VFD with the 2 provided M5 T-nuts and bolts. Insert them along the same horizontal t-slot. The fasteners are slightly long, so they can extend from the t-slot and serve as a perch to hook the VFD in to for easy access.

| ![VFD mounting](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/acmotor-techdoc-3-compressed.png) ***VFD mounting*** |
| --- |

## Connecting Electronics

Internally, both the AC motor and VFD come pre-wired and configured for basic motor operations. To complete the electrical installation, follow the wiring diagram below:

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI - VFD - AC Motor1.png) ***Motor, VFD and Digital IO Wiring*** |
| --- |

## Controlling and programming the VFD

The Lenze VFD is an extremely feature-rich frequency drive allowing for highly configurable control and motor operation. This is possible through modifying and configuring so-called parameters. Parameters are values, stored in the VFD, that control how the motor and VFD behave. Most of the parameters needed for basic function are pre-set and do not need changing.

You can perform operations using the VFD keypad, as described in the table below.

| ![Table 1: Keypad controls](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/vfd-keypad-buttons-table(1).png) ***Table 1: Keypad controls*** |
| --- |

However, you may need to manually configure some parameters if you are modifying motor operating characteristics or setting up certain digital inputs.

To change a parameter:

1. Press **Enter** briefly.
2. With the up and down arrow keys, select the group the parameter is in. Parameters are formatted as PXYY.ZZ, where the first digit after P indicates the group. (For example, parameter P400.01 is in group 4.) Press **Enter**.
3. With the up and down arrow keys, select the parameter. Press **Enter**.
4. With the up and down arrow keys, change the parameter value. Press **Enter** to input the change.
5. To save the new parameter value, press and hold **Enter** for at least three seconds.

Caution: Incorrect parameters can damage the motor or VFD.

## Starting and stopping the motor

You can control the motor directly from the VFD - which is the default, manual option or through MachineMotion, which requires further integration.

### Enabling VFD keypad control

1. Press **CTRL** briefly. The screen displays ”Keypad Full CTRL?” and then indicates the desired state (e.g.: “ON” will be displayed as the desired state).
2. Press **Enter** briefly to change from OFF to ON. A red error light will begin to flash when keypad control is enabled, this is normal.

### Control via VFD keypad

To control the motor directly from the VFD, press the following buttons:

1. **(I)** key. Start motor, press briefly.
2. **UP and DOWN** arrow keys. Change frequency (motor RPM). There is no direct RPM feedback.
3. **R-F** key. Change directions.
4. **(0)** key (in red). Stop motor.

### Control via MachineMotion

To control the motor remotely via MachineMotion, you will need to set up remote triggering of digital inputs (such as a start-stop function). This requires a MachineMotion, the Digital IO Module ([CE-MD-001-0000__2](https://vention.io/parts/digital-io-module-v2-1464)) and M12 Cable for Digital I/O Module v2 - Female to 3x Female (5m) ([CE-CA-051-5000](https://vention.io/parts/m12-cable-for-digital-io-module-v2-female-to-3x-female-5m-1756)), all sold separately.

The AC Motor and VFD is an actuator controlled via digital outputs. Therefore your VFD will not be stopped by the system upon an emergency stop event. It is important to note that it is NOT a safety rated actuator. If you would still like to see the VFD stop upon an emergency stop event, please contact the Customer Success team.

**VFD Configuration**

The following guide will run through the example of setting up the “start-stop” and “forward-reverse” digital inputs:

1. Establish the connection of the Digital I/O module to the MachineMotion via any of the four available control ports.
2. Connect the triple splitter cable as follows:
  1. Connector labeled **Red** to Digital Output 0 (start-stop trigger)
  2. Connector labeled **Blue** to Digital Output 1 (reverse trigger)
  3. Connector labeled **Green** is not used
3. Establish the connection with the splitter cable to the VFD as seen above.
4. With the VFD keypad control enabled, navigate to parameter menu **P210.00**, which is the minimum motor frequency. It is natively set to 0 Hz, however will be required to be set at the desired operating frequency. Set the desired value using the **UP** and **DOWN** arrow keys and press **Enter** once the desired value is achieved.
5. Return to the main menu and disable keypad control. Note the displayed text on the screen indicating “KSTOP”.
6. Press the motor start button **(I)**. It should now read “STOP”. You are now ready to control the VFD from Control Center.
7. Connect your laptop to the MachineMotion’s “To PC“ port, open the Chrome browser, and navigate to the following URL : `machinemotion.local`
8. In Control Center, under Manual Control, enable Digital Output 0, the motor should spin up to the previously set frequency.
9. With Digital Output 0 still triggered, enable Output 1, the motor should decelerate and reverse direction back up to the previously set frequency.

For a list of additional available digital inputs and a step-by-step programming guide, see Lenze’s i510 commissioning guide, section 6.2: [lenze.com](https://www.lenze.com/en-ca/products/inverters/frequency-inverters/i510-protec-frequency-inverter).

If you have any questions or concerns about configuring VFD parameters, Vention’s customer success team can assist with troubleshooting.

## M12 S-Key 4 pins Female Connector

| Pin | Description |
| --- | --- |
| Pin 1 | Phase U |
| Pin 2 | Phase V |
| Pin 3 | Phase W |
| Pin 4 | EARTH |

## M12 A-Key 5 pins Male Connector

| Pin | Description |
| --- | --- |
| Pin 1 | VFD Input 1 |
| Pin 2 | VFD Input 2 |
| Pin 3 | 0V |
| Pin 4 | VFD Input 3 |
| Pin 5 | Not Connected |

## Documentation for Previous Product Versions

****AC Motor and VFD for Material Handling****

[AC Motor and VFD for Material Handling](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/AC%20Motor%20and%20VFD%20for%20Material%20Handling.pdf)