---
title: "Safety Modules Use Case Reference Guide"
slug: "safety-modules-use-case-reference-guide"
updated: 2026-01-08T17:12:56Z
published: 2026-01-08T17:12:56Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Safety Modules Use Case Reference Guide

| ![Cover image of technical document](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/safety-modules-blog-1.png) |
| --- |

### Overview

Welcome to the Safety Modules Use Case Reference Guide. Here, you’ll find all the information you need to seamlessly integrate Vention’s safety devices into your machine design, based on your specific use case. Please note, to ensure proper functionality, insert a black jumper into any unused DEVICE connectors on any of the safety modules. Yellow jumpers are reserved for unused Safety IN of the safety modules and MachineMotion AI.

> [!WARNING]
> This document covers the latest version of Vention’s Safety Modules Use Case Reference Guide. For previous version, refer to link below:
> 
> [*Documentation for Previous Product Versions*](/technicaldocumentation/docs/safety-modules-use-case-reference-guide#documentation-for-previous-product-versions)

  

### Scenario #1: Replacing a part inside a machine with light curtains without triggering an e-stop

**Problem**: You have Vention equipment and need to manually feed and outfeed parts. You want the e-stop to trigger if the light curtains are activated while the machine is operating. Additionally, you want the light curtains to be disabled once the cycle is complete, allowing the operator to replace the part (e.g., glue dispensing machine, sanding cell, machine tending, etc.).

**Solution**: The Mode Switching Safety Module AI ([CE-SA-018-0001__2](https://vention.io/parts/mode-switching-module-ai-3193)) is tailor-made for these requirements. It seamlessly links light curtains and other safety devices, ensuring smooth operation and providing emergency stop functionality when necessary.

| ![Figure 1 - Example of a machine that could use the mode switching safety module](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Man20with20machine.png) ***Figure 1 - Example of a machine that could use the mode switching safety module*** |
| --- |
| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with Mode Switching &amp; safe sensor.png) ***Figure 2 - Mode switching safety module wiring diagram*** |

  

### Scenario #2: Robot automatically returns to normal operation when the area scanner-defined collaborative speed zone is not triggered

**Problem**: Machine tending cell with a cobot, and you want to only use area scanners. A first zone will slow the robot down to a collaborative speed, while stepping out of the collaborative zone resumes the robot to move at full speed.

**Solution**: Combine the Datalogic Laser Area Scanner (PR-DA-201-0489) with the Auto-reset Safety Module AI ([CE-SA-019-0001__2](https://vention.io/parts/auto-reset-module-ai-3194)) and Robot Safety Module AI ([CE-SA-016-0001__2](https://vention.io/parts/robot-safety-module-ai-3190)). The laser scanner’s OSSD 1, 2, and 3 are connected to the auto-reset module device ports. The reduced speed port of the auto-reset module is connected to the reduced speed port of the robot safety module. This setup allows the scanner to automatically return to full speed when an operator exits the collaborative zone.

| ![Diagram showing components of a robotic safety system with labeled connections and modules.](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Robot Safety Module wiring diagram with Auto-Reset Module (CE-SA-019-0001__2) with callouts(1).png) ***Figure 3 - Auto-Reset Safety Module AI wiring diagram - Standard reset*** |
| --- |

### Scenario #3: Collaborative speed control with auto-reset and defined e-stop zone

**Problem**: Machine tending cell with a cobot on a range extender and you want to only use area scanners. A first zone will decelerate the robot to a collaborative speed. If someone moves beyond that zone, the robot halts entirely. Entering the collaborative zone and then stepping out resumes normal operation (provided you don’t enter the e-stop zone).

**Solution**: In addition to all the modules in scenario #2 you will need the Muting Safety Module AI ([CE-SA-015-0001__2](https://vention.io/parts/muting-safety-module-ai-3189)).

| ![Diagram showing robot components including safety modules, cables, and controllers for automation.](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Auto-reset with defined e-stop zone wiring diagram with callouts(1).png) ***Figure 4 - Auto-reset with defined e-stop zone wiring diagram*** |
| --- |

### Scenario #4: Access control for machine cells (no robot)

**Problem**: Ensure that your system is in a safe state before being able to open the door. You aim to press a button that triggers the homing sequence and then unlocks the system.

**Solution**: Utilize the Access Request Module AI ([CE-SA-017-0001__2](/technicaldocumentation/docs/access-request-module-ai-datasheet)) to manage access to your machine, providing peace of mind and security.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with ARM with 4x interlocks with callouts.png) ***Figure 6 - Access Request wiring diagram with four guardlocks*** |
| --- |

### Scenario #5: Access control for machine cells (with robot)

**Problem**: Ensure that your system is in a safe state before being able to open the door. You aim to press a button that triggers the homing sequence and then unlocks the system.

**Solution**: Utilize the Access Request Module AI ([CE-SA-017-0001__2](https://vention.io/parts/access-request-module-ai-3192)) to manage access to your machine and a Smart Robot Safety Module AI ([CE-SA-016-0001__2](https://vention.io/parts/robot-safety-module-ai-3190)) connected to your robot. The Robot Safety Module should be the last module in the safety chain connected to the MachineMotion.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI with ARM &amp; RSM &amp; 2x Interlocks with callouts(1).png) ***Figure 7 - Access Request wiring diagram with robot with two guardlocks*** |
| --- |

### Scenario #6: Muting light curtains for conveyor systems

**Problem**: Prevent boxes from triggering e-stops while using light curtains. You would like to mute light curtains when boxes are exiting or entering.

**Solution**: Combine the Muting Safety Module AI ([CE-SA-015-0001__2](https://vention.io/parts/muting-safety-module-ai-3189)) with proximity sensors ([CE-AP-002-0000__2](https://vention.io/parts/safety-module-muting-kit-2952)) for effective management of light curtain signals.

- Connect the light curtain to either port Device 3 or Device 4.
- Use Muting sensor Y adapters (CE-SA-107-0001). Connect two sensors to port XA and the other two to port XB.
- One sensor connected to port XA and 1 sensor connected to XB are placed on one side of the light curtain. The two remaining sensors are placed on the other side of the light curtain.

The distance between the sensors should be established based on the following information:

- Less than 2 seconds between activation of XA and XB.
- The distance between the two pairs of sensors is less than the length of the boxes.
- Muting ends after 10 seconds.

| ![Figure 8 - Example of the muting use case](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Box20on20conveyor20with20muting.gif) ***Figure 8 - Example of the muting use case*** |
| --- |
| ![Diagram showing Keyence light curtains, safety modules, and connection cables for machine safety.](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Muting kit wiring diagram with callouts.png) ***Figure 9 - Muting kit wiring diagram*** |

### Scenario #7: Managing multiple robots in a cell

**Problem**: You have multiple robots in the same cell, and when you e-stop one, you would like the other robots in the cell to stop, too.

**Solution**: Custom safety modules are necessary for effectively managing multiple robot applications. Contact us to define a proper solution.

  

## Commissioning checklist

We’re pleased to provide you with comprehensive commissioning checklists for the safety modules you’ve invested in. These checklists serve as valuable resources to ensure the seamless integration and optimal performance of your safety systems.

You can access the commissioning checklists through the following links:

[Muting Safety Module AI](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/CE-SA-015-0001__2_Commissioning%20checklist.pdf) [Mode Switching Safety Module AI](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/CE-SA-018-0001__2_Commissioning%20checklist.pdf) [Auto-Reset Safety Module AI](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/CE-SA-019-0001__2_Commissioning%20checklist.pdf) [Robot Safety Module AI](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/CE-SA-016-0001__2_Commissioning%20checklist.pdf) [Access Request Module AI](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/CE-SA-017-0001__2_Commissioning%20checklist.pdf)

---

## Documentation for Previous Product Versions

**Safety Modules Use Case Reference Guide**

[Safety Modules Use Case Reference Guide](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Safety%20Modules%20Use%20Case%20Reference%20Guide.pdf)

We’re committed to ensuring your workplace safety with our comprehensive range of safety devices. For more details and assistance, visit [Vention’s Safety Device Collection](https://vention.io/parts-library?category=SA#f-ec_category=SA).