Belt Rack Actuator
Motion Parts › Linear Motion
… of tension. This ensures that new rack segments are aligned properly. Repeat step 11 until all rack segments are attached. Attach the second belt clamp. Tighten the idler set screws on the housing to approximately 1Nm. Cycle the actuator and check that it runs smoothly, increase or decrease the tension until the actuator runs smoothly. Attach the motor or powertrain components. Notes: When installing motors, apply a small amount of grease to the motor shaft so that it is lightly coated. This will reduce the possibility of fretting corrosion occurring during operation, making future removal easier. Moreover, do not use excessive force (hammering, prying or using screws to “push” the motor) to install the motor. 16. Attach any accessories, such as sensors or end stops. Maintenance For maintenance instructions, please see the maintenance tech doc. Documentation for Previous Product Versions Belt Rack Actuator Datasheets MachineMotion V2 Belt Rack Actuator Datasheet