---
title: "Timing Belt Actuator"
slug: "timing-belt-actuator"
updated: 2026-06-02T13:18:08Z
published: 2026-06-02T13:18:08Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Timing Belt Actuator

| ![Cover image of technical document](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/belt-driven.png) |
| --- |

## Overview

Belt-driven linear actuators are typically used for light to medium duty applications that require higher speeds and acceleration. Consisting of two concealed timing belt pulleys mounted at the ends of a Vention 45 x 90 mm extrusion, the assembly can accommodate any of Vention’s Nema 34 stepper motors and comes in a variety of lengths.

> [!WARNING]
> This document covers requirements for current version of MachineMotion controller. For previous version, refer to link below:
> 
> [Documentation for Previous Product Versions](/technicaldocumentation/docs/timing-belt-actuator#documentation-for-previous-product-versions)

## Compatible Guides

The belt-driven linear actuator can drive a variety of gantries that are in turn supported by both Eccentric and Concentric V-shaped rollers (MO-LM-001-[0027](https://vention.io/parts/gf-nylon-eccentric-roller-330)/[0028](https://www.vention.io/parts/331)) or linear bearings on shafts ([MO-LM-014-XXXX](https://vention.io/parts/16mm-shaft-for-linear-bearings-585mm-1471)). Both configurations can be seen below.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/og_timingbelt-config.png) ***Exhibit 1. Belt-driven linear actuator shown with medium gantry and nylon V-shaped wheels*** ***Exhibit 2. Belt-driven linear actuator shown with medium gantry and linear bearings and shafts*** |
| --- |

## Applications

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/og_timingbelt-app.png) |
| --- |

There are several application for belt-driven linear actuators, including a UR10 7th Axis or a 3-Axis Palletizer.

## Technical Specifications

| Available Lengths | 585mm to 1530mm in 45mm increments + 1980mm, 2295mm Net displacement is equivalent to the extrusion length minus the gantry’s longitudinal dimension |
| --- | --- |
| Displacement Ratio (mm/turn) | 150 |
| Linear Force / Torque Ratio (N/Nm) | 42 |
| Maximum input torque (Nm) | 61 |
| Output Force Capacity (N) | See Exibit 3 & 4 below |
| Repeatability including backlash (mm) | ±0.3 |
| Total Backlash (mm) | 0.25 |
| Back Drive Resistance | Low |
| Motor Compatibility | NEMA 34, 14mm shaft MO-SM-030-0001, MO-SM-030-0002, MO-SM-030-0003 |
| Sensor Compatibility | Compatible with all M18 sensors using the left or right end stops(MO-LM-015-0001/0002) |
| Belt Life (hours) | 6000-11000 |

### Inertia Ratio

#### Calculating Inertia Ratio

$Inertia\;Ratio = \frac{Actuator\; Inertia}{Motor\; Inertia} * \frac{1}{(Gearbox\; Ratio)^{2}}$

$Actuator\;Inertia = 5.6993*10^{-4}*(m+0.164kg+external\; hardware)$

$where\; m\; is\; the\; applied\; mass\; to\; the\; gantry\; [kg]$

$external\; hardware\; refers\; to\; bearing\; or\; guides,\; fasteners\; and\; motor\; combined\; moving\; mass\; [kg]$

Vention servo motor inertia values:

- MO-SM-030-0003: 3.74×10⁻⁴ kg*m²
- MO-SM-030-0002: 1.48×10⁻⁴ kg*m²
- MO-SM-030-0001: 0.915×10⁻⁴ kg*m²

**Sample Calculation**

Timing belt actuator, with a 5:1 gearbox, moving 40kg (5kg of external hardware), driven by a large motor.

$Inertia\;Ratio = \frac{Actuator\; Inertia}{Motor\; Inertia} * \frac{1}{(Gearbox\; Ratio)^{2}}= \frac{5.6993*10^{-4}*(40kg+0.164kg+5kg)}{3.74*10^{-4}kg*m^{2}} * \frac{1}{(5)^{2}}=2.75$

**Note:**For most applications, an **inertia ratio of 100:1 or lower** is recommended. Adding a gearbox will help reduce the ratio. Generally, lowering the inertia ratio of a system results in a better response/control. If your application exceeds the recommended 100:1 inertia ratio, we encourage you to contact our Application Engineering team for a technical assessment of its feasibility.

The figure below demonstrates the linear force output in function of the linear speed of the belt-driven linear actuator. This was calculated using Vention’s NEMA 34 stepper motors driven by MachineMotion 2.

| ![Graph showing the relationship between force and speed for a timing belt.](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI-Timing-Belt-August6-I2T.png) ***Exhibit 3. Force in function of linear speed using Vention NEMA 34 stepper motors*** |
| --- |

Observing the figure above, the force slowly decreases as the linear velocity increases, making the timing belt actuator ideal for lower force applications that require higher movement speeds. If more force is required and travel speed is not as critical, consider adding a gearbox to the powertrain. See the below figure for expected performance with a gearbox.

| ![Graph showing the relationship between force and speed for a timing belt system.](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/MMAI-Timing-Belt-5-August6-I2T.png) ***Exhibit 4. Force in function of linear speed using Vention NEMA 34 stepper motors and a 5:1 reduction gearbox.*** |
| --- |

Observing the figure above, the force is much higher when using the gearbox, however it decreases much faster as the linear velocity increases. This makes the combination ideal for slower moving applications with higher forces.

**Notes**:

- These performance curves are made with our motors and controller at steady state conditions. Using others motors or controllers will have different behavior therefore performance and reliability cannot be guaranteed.
- These performance curves are valid assuming a 100:1 inertia ratio or lower.
- Performance curves represent peak torque and speed values. Actual continuous performance may be lower due to I²t protection in the driver. For applications involving continuous, sustained torque output, contact Vention support for thermal derating guidelines or continuous-duty application advice.
- Motors are equipped with an integrated safety mechanism known as **I²T protection**, which prevents overheating. This function continuously monitors the current drawn by the motor over time. If the motor operates at full load for an extended period (approximately 40–60 seconds), the I²T protection engages and limits the current, thereby reducing the available torque. The dashed lines in the graph illustrate the motor’s performance under these conditions. Once the motor has cooled sufficiently, it automatically returns to normal operating mode.
- When two motors are mounted **on the same actuator** and operated in **Cyclic Synchronous Torque (CST)** mode, an increase in actuator output force of 1.8× can be expected. This performance gain is only applicable when **both motors are synchronized in CST mode**. Motors that are synchronized—but not operating in CST mode—**do not** yield this increase.

#### Selecting the right motion parameters

1. **Determine motion requirements:** Start by defining the load that needs to be moved and the required acceleration using basic kinematic equations.
2. **Calculate required force:** Apply Newton’s second law (F = m * a) to determine the resultant force the actuator must provide.
3. **Reference performance curves:** On the Force vs Speed graphs, locate the maximum achievable speed corresponding to the required force.

If operation is near the limits of the performance curve and you observe non-smooth motion or excessive following error (discrepancy between requested position and actual position), reduce the requested speed and/or acceleration. Lowering these values decreases system demand, which improves control stability and motion quality. Reducing the inertia ratio may also help the system response (see below).

## Assembly Instructions

### Motor Installation

The Timing Belt Actuator comes pre-assembled with the only remaining task of installing the selected powertrain components and guiding system.

To connect powertrain components (stepper motor, brake and gearbox), perform the following steps:

- Remove the motor cover on the actuator endblock, to install the stepper motor.
- Optional: If you have a brake or gearbox, connect them to the output shaft of the stepper motor using the provided M6 X 20mm fasteners.
- Connect your stepper motor to the actuator using x4 M6 X 20mm fasteners (HW-FN-005-0020).

**Notes:**

- **When installing motors, apply a small amount of grease to the motor shaft so that it is lightly coated. This will reduce the possibility of fretting corrosion occurring during operation, making future removal easier.**
- **Moreover, do not use excessive force (hammering, prying or using screws to “push” the motor) to install the motor.**

### Linear Guide Installation

Install the guiding system and gantry plate of your choice. If using linear guide rails, install both rails followed by sliding the bearing carriages on the guide rails and finally attaching the bearings together using a gantry plate. Be careful to use the short M8 fasteners included with the bearings or the cartridge can be damaged.

If using roller wheels, attach the roller wheels to the gantry plate while it is in place on the extrusion. Adjust the eccentric rollers until there is no lateral play but rolling motion is still smooth.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/og_timingbelt-config.png) |
| --- |

Finally, attach the belt tensioner to a counterbore in the middle of your gantry plate.

### Sensor Installation

Sensors can be installed in four configurations on the actuator using the Left/Right Timing Belt Sensor Bumper (MO-LM-015-0001/0002). To install a sensor, screw the sensor all the way into the hole until it bottoms out. Install one jam nut on either side of the sensor and tighten them to lock the sensor in place.

Note: The only sensor compatible with the actuator is the non-flush inductive proximity sensor (CE-SN-004-0001).

### Tensioning

To tension the timing belt, locate the two screw heads under the gantry and use a hex key to tighten both screws equally until desired belt tension is reached.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/og_timingbelt-tension.png) |
| --- |

## Documentation for Previous Product Versions

****Timing Belt Actuator Datasheets****

[MachineMotion V2 Timing Belt Actuator Datasheets](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Timing%20Belt%20Actuator.pdf)