---
title: "Worm Gearbox"
slug: "worm-gearbox"
updated: 2025-11-26T19:44:42Z
published: 2025-11-26T19:44:42Z
---

> ## Documentation Index
> Fetch the complete documentation index at: https://docs.vention.io/llms.txt
> Use this file to discover all available pages before exploring further.

# Worm Gearbox

## Overview

This guide covers the setup and specifications of the Vention gearbox assembly. This assembly includes a 70:1 gearbox and a 200mm handwheel for precise manual control. All parts are designed for seamless interfacing with the Vention ecosystem.

Two kit options will be detailed:

- A right angle gearbox attachment to allow for the input axis to be parallel with the output axis (MO-RM-007-1000)
- An additional support for the output shaft to allow for increased payload (MO-RM-007-0010)

## **Assembly & Specifications:**

## **MO-RM-007-0000 Worm Gearbox Kit, 70:1 Ratio:**

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Studio 857F-5153.png)

### **Kit Contents:**

- 1x Worm Gearbox; - 1x Hand Wheel; - 1x Flanged Output Shaft Assembly; - 1x Gearbox Attachment Block; - 4x M8×18 screws; - 1x M6×16mm screw; - 6x M8×65mm screws.

### **Installation Instructions**

- **Mount the plate**: Bolt the base plate to the extrusion structure.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(471).png)
- **Secure the gearbox**: Fasten the gearbox to the mounting plate using either a****ball-end Allen key, a ball-end t-handle or a stubby hex key to easily reach the bolts.

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(472).png) | ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1761922459469.png) |
| --- | --- |
- **Install the hand wheel:** Slide the hand wheel onto the input shaft of the gearbox. Fasten it using the provided washer and M6 × 16mm screw to prevent the hand wheel from sliding off.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1761932313873.png)
- **Line up the keys**: The end of the shaft has small raised rectangular parts called keys. They must be lined up with the matching grooves, or keyways, inside the gearbox opening.
- **Slide it In**: Once those keys and grooves are aligned, push the shaft into the gearbox. The shaft can be slid in from either side of the gearbox, both orientations are supported.

![Should this have the aluminum plate with the handwheel that the render above has?](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(417).png)
- **Seat It firmly**: Continue pushing the shaft until the stepped section is fully seated.
- **Lock It down**: Slide the provided shaft collar onto the exposed end of the shaft. The collar can then be secured by tightening the two fasteners to a torque between 9 and 11 Nm. This will ensure that the shaft cannot slide out of the gearbox assembly.
- **Discard plate**: Once you are done, you will be left with one extra plate with the part number MO-RM-007-0002, this is normal and the plate is to be discarded.

### **Technical Specifications**

|  |  |
| --- | --- |
| Ratio | 70:1 |
| Maximum Output Torque* [Nm] (MA) | 58 |
| Output Radial Load [N] | 4200 |
| Output Axial Load [N] | 840 |
| Maximum Payload with MO-RM-007-0010 [kg] | 453 |
| Maximum Payload without MO-RM-007-0010 [Nm] (MB) | 400 |

**Exceeding this output torque will reduce the life of the gears. Please consult our Application Engineering department for any additional information.*

| ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1764183546968.png) | ![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1764183523351.png) |
| --- | --- |

## **MO-RM-007-1000 Right Angle Input Kit for Worm Gearbox:**

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/Studio Set-852b-5094.png)

### **Kit Contents:**

- 1x Worm Gearbox; - 1x Hand Wheel; - 1x Flanged Output Shaft Assembly; - 1x Gearbox Attachment Block; - 4x M8×18 screws; - 1x M6×16mm screw; - 6x M8×65mm screws; - 1x M5×16mm screw; - 1x Right Angle Gearbox, 1:1.

### **Kit Contents:**

### **Installation Instructions**

To begin, follow the installation instructions listed under MO-RM-007-0000 Worm Gearbox Kit, 70:1 Ratio in the section above but skip the step instructing to install the hand wheel on.

- **Remov****e hardware:** Locate the input shaft on the main gearbox. Remove and discard the 6 M6 screws located around the input shaft of the worm gearbox.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1761934076220.png)
- **Install the adaptor plate:** Take the right angle adaptor plate and align the mounting holes with the matching set on the gearbox. Use the six M6 × 60mm screws provided in the kit to securely bolt the adaptor plate into position. Torque these screws in a star pattern to a torque between 9 and 11 Nm.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(419).png)
- **Slide the right-angle gearbox on:** Carefully slide the right angle gearbox onto the exposed shaft of the gearbox kit. Use the four M6 × 20mm fasteners provided to secure the right angle gearbox to firmly to the adaptor plate.

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image(420).png)
- **Install the hand wheel:** Slide the hand wheel onto the shaft of the 1:1 right angle gearbox. Fasten it using the provided washer and M5 × 16mm screw to prevent the hand wheel from sliding off.

## **MO-RM-007-0010 Self Aligning Rotary Jig Support:**

![](https://cdn.document360.io/3eee4d14-5ca0-4ea6-b426-1c19393e6a5e/Images/Documentation/image-1760645813675.png)

This self-aligning support can be used to compensate for small shaft misalignment errors of less than **2.5 degrees** during installation. The support can be mounted to the Vention extrusion and accommodates the mounting pattern as the flange output shaft assembly.

If the shaft is too far off-axis (over 2.5 degrees), the bearing seals may pop out. If this happens, they can be easily pressed back into the bearing by hand.

### Technical Specifications

|  |  |
| --- | --- |
| Maximum Misalignment [degrees] | 2.5 |
| Maximum Payload [kg] | 225 |
| Maximum Rotation Speed [RPM] | 18000 |
| Maximum Dynamic Radial Load [kN] | 14.3 |
| Maximum Static Radial Load [kN] | 4.0 |
| Worm Gearbox (MO-RM-007-0000) Maximum Payload with this support [kg] | 453 |