Overview
This document details the commands that can be sent to your MachineMotion AI using Ethernet TCP/IP protocol. It is supported on MachineMotion software version v3.1.0 and newer versions. This API uses sockets to exchange data. All information is packaged in string format and sent over the socket communication channel to port 9999 of the MachineMotion AI.
The TCP Socket API is a TCP server that enables a TCP client to :
Get information about the status of the MachineMotion
Get information and send commands to motors connected to the MachineMotion
Set outputs and read inputs of the IO modules connected to the MachineMotion
Send and receive custom messages over the mqtt broker of the MachineMotion
For details on previous releases of Vention’s Low-Level Socket Programming Interface with MachineMotion 2 and MachineMotion 1, refer to the Documentation for Previous Product Versions section at the end of this document.
Configuring an IP Address
See MachineMotion AI Controller User Manual to learn more about how to configure the IP address of the MachineMotion.
A connection must be opened before any commands can be sent or received from the MachineMotion. How to open a connection will depend on the programming language being used.
Using the TCP Socket API
End of Line character
This feature is present on the MachineMotion AI release v3.2.0 and newer.
Each message exchanged on the TCP Socket API must end with /n .
This will be the case of the payload received, and sent.
Heartbeat
This feature is present on the MachineMotion AI release v3.2.0 and newer.
Heartbeat message
To ensure that the TCP connection is alive, make sure that no more than 0.5s span between each message.
If no message has been received by the MachineMotion within 0.5s, the MachineMotion will initiate a disconnection.
Instead of sending one of the commands listed below, you could send a heartbeat message:
Heartbeat
Description
Message exchanged to keep the TCP connection alive. This is a no-operation on the MachineMotion side.
Format
ping
Usage
ping will have the MachineMotion keep the TCP connection alive for another 0.5s.
Response
pong
Quickstop on disconnection
Upon the socket disconnecting, the MachineMotion will stop the motion of all its connected motors.
You can deactivate this behaviour using the setQuickStopOnDisconnect command.
Set Quickstop on Disconnect
Description
Sets wether or not to stop the motion of all motors upon a socket disconnection event.
Format
setQuickStopOnDisconnect_<Payload>
Where <Payload>> can be:
0to not stop all the motors upon a socket disconnection1to stop all motors upon a socket disconnection. This is the default behaviour of the MachineMotion.
Usage
setQuickStopOnDisconnect_0 will change the default behaviour of the MachineMotion. Upon a socket disconnection, the motors won’t stop their on-going motion.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
List of Commands
Get Safety State
Description
Returns the safety state of the MachineMotion.
Format
getSafetyState
Usage
getSafetyState
Response
The safety state of the MachineMotion can be one of those values:
-1corresponds to an error in the safety state0corresponds to no safety state (this would be the case for the MachineMotion AI Robot and MachineMotion AI Robot Pro models)1corresponds to an emergency stop state2corresponds to a normal safety stateERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Operational State
Description
Returns the operational state of the MachineMotion.
Format
getOperationalState
Usage
getOperationalState
Response
The operational state of the MachineMotion can be one of those values:
1corresponds to operational0corresponds to non-operationalERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Enable Operation
Description
Request the MachineMotion to change its operational state to be operational again.
Format
operationEnable
Usage
operationEnable
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Disable Operation
Description
Request the MachineMotion to change its operational state to not be operational.
Format
operationDisable
Usage
operationDisable
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Move
Description
Moves an axis immediately, to a given position, distance or speed.
Format
move_<Payload>;*
Where <Payload>> corresponds to a TrapezoidalMove or a ContinuousMove .
Note : ;* means multiple can be input in the same request.
A - Trapezoidal Move
Moves an axis immediately to a given position or by a given distance.
Fields can be specified in any order.
Field | Description | Is Mandatory |
|---|---|---|
| The move type | yes |
| Is the motion relative or absolute | yes |
| The motor address (port and index) and its target position for absolute moves, or its target distance for relative moves. | yes |
| Desired velocity, in mm/sec | yes |
| Desired acceleration, in mm/sec2 | yes |
| NOT USED (Desired deceleration) | no |
| NOT USED (Jerk value of the move) | no |
| Ignore the synchronization configuration of parent and child motors | no |
B - Continuous Move
Moves a conveyor or rotary table axis continuously at a given speed and acceleration.
Fields can be specified in any order.
Field | Description | Is Mandatory |
|---|---|---|
| The move type | yes |
| The motor address (port) | yes |
| The motor address (index) | yes |
| Desired velocity, in mm/sec. | yes |
| Desired acceleration, in mm/sec2 | yes |
Usage
move_type:trapezoidal,[port:1,index:1,target:300],velocity:300,acceleration:100,relative:1 starts moving the first motor connected to port 1, by a distance of 300 mm, with a velocity of 300 mm/sec, and an acceleration of 100 mm/sec2.
move_type:continuous,port:1,index:1,velocity:300,acceleration:100 starts moving the first motor connected to port 1, continuously at a velocity of 300 mm/sec, with an acceleration of 100 mm/sec2.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Add Move
Description
Adds a move to list of moves, to be executed later, when the command moveGo will be sent.
It will enable moving an axis to a given position, distance or speed, later on.
Format
moveAdd<Payload>;*
Where <Payload> corresponds to a TrapezoidalMove or a ContinuousMove .
Note : ;* means multiple can be input in the same request.
A - Trapezoidal Move
Moves an axis to a given position or by a given distance.
Fields can be specified in any order.
Field | Description | Is Mandatory |
|---|---|---|
| The move type | yes |
| Is the motion relative or absolute | yes |
| The motor address (port and index) and its target position for absolute moves, or its target distance for relative moves. | yes |
| Desired velocity, in mm/sec | yes |
| Desired acceleration, in mm/sec2 | yes |
| NOT USED (Desired deceleration) | no |
| NOT USED (Jerk value of the move) | no |
| Ignore the synchronization configuration of parent and child motors | no |
B - Continuous Move
Moves a conveyor or rotary table axis continuously at a given speed and acceleration.
Fields can be specified in any order.
Field | Description | Is Mandatory |
|---|---|---|
| The move type | yes |
| The motor address (port) | yes |
| The motor address (index) | yes |
| Desired velocity, in mm/sec | yes |
| Desired acceleration, in mm/sec2 | yes |
Usage
moveAdd_type:trapezoidal,[port:1,index:1,target:300],velocity:300,acceleration:100,relative:1 will queue up a motion that starts moving the first motor connected to port 1, by a distance of 300 mm, with a velocity of 300 mm/sec, and an acceleration of 100 mm/sec2.
moveGo will start executing the previously described move.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Go Move
Description
Will start the execution of all the moves that have been queued up by the moveAdd command.
Format
moveGo
Usage
moveAdd_type:trapezoidal,[port:1,index:1,target:300],velocity:300,acceleration:100,relative:1 will queue up a motion that starts moving the first motor connected to port 1, by a distance of 300 mm, with a velocity of 300 mm/sec, and an acceleration of 100 mm/sec2.
moveGo will start executing the previously described move.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Clear Move
Description
Will clear all the moves that have been queued up by the moveAdd command, without executing them.
Format
moveClear
Usage
moveAdd_type:trapezoidal,[port:1,index:1,target:300],velocity:300,acceleration:100,relative:1 will queue up a motion that starts moving the first motor connected to port 1, by a distance of 300 mm, with a velocity of 300 mm/sec, and an acceleration of 100 mm/sec2.
moveClear will start clear the previously described move. It will not be executed by any subsequent moveGo command.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Move Home
Description
Moves an axis immediately, towards its home position, until the home sensor is triggered. This will reset the zero position of the axis.
Format
moveHome_<Payload>;*
Where <Payload>> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Note : ;* means multiple can be input in the same request.
Usage
moveHome_1,1 starts moving the first motor connected to port 1, towards its home sensor.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Add Move Home
Description
Adds a homing move to list of homing moves, to be executed later, when the command moveHomeGo will be sent.
It will enable moving an axis towards its home position, until the home sensor is triggered. This will reset the zero position of the axis.
Format
moveHomeAdd_<Payload>;*
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Note : ;* means multiple can be input in the same request.
Usage
moveHomeAdd_1,1;2_1 will queue up a motion that will start moving the first motor connected to port 1, as well as the first motor connected to port 2, towards their home sensors.
moveHomeGo will start executing the previously described move.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Go Move Home
Description
Will start the execution of all the moves that have been queued up by the moveHomeAdd command.
Format
moveHomeGo
Usage
moveHomeAdd_1,1;2_1 will queue up a motion that will start moving the first motor connected to port 1, as well as the first motor connected to port 2, towards their home sensors.
moveHomeGo will start executing the previously described move.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Clear Move Home
Description
Will clear all the moves that have been queued up by the moveHomeAdd command, without executing them.
Format
moveHomeClear
Usage
moveHomeAdd_1,1;2_1 will queue up a motion that will start moving the first motor connected to port 1, as well as the first motor connected to port 2, towards their home sensors.
moveHomeClear will start clear the previously described move. It will not be executed by any subsequent moveHomeGo command.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Quick Stop
Description
Immediately stops motion on the given axes.
Format
quickStop_<Payload>;*
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Note : ;* means multiple can be input in the same request.
Usage
quickStop_1,1;2,2 will immediate stop any motion on the first motor connected to port 1, and the second motor connected to port 2.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Set Position
Description
Sets the current position of an axis to a new value. It does not move the axis.
Format
setPosition_<Payload>
Where <Payload> corresponds to <port>, <index>,<position> :
<port>is the motor address (port)<index>is the motor address (index)<position>is the new position value, in mm.
Usage
setPosition_1,1,1000 Sets the current position if the first motor connected to port 1 at position 1000 mm.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Set Ignore End Sensors
Description
Sets whether or not the axis should ignore the status of its end of travel sensors during a move.
Format
setIgnoreEndSensor_<Payload>
Where <Payload> corresponds to <port>, <index>,<[0,1]> :
<port>is the motor address (port)<index>is the motor address (index)<[0,1]>1 corresponds to ignoring them, 0 corresponds to take them into account. By default, they won’t be ignored.
Usage
setIgnoreEndSensor_1,1,0 Sets the the first motor connected to port 1 to not ignore its end of travel sensors.
Response
1corresponds to a successERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Connected
Description
Queries the connection status of a motor: whether or not it is currently detected as available hardware by the MachineMotion.
Format
getConnected_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getConnected_1,2 returns whether or not there is a motor detected on port 1, in second position in the motor chain.
Response
1corresponds to a motor being detected at the given address0corresponds to no motor being detected at the given addressERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Position
Description
Queries the current position of a motor.
Format
getPosition_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getPosition_1,1 returns the position of the first motor connected to port 1.
Response
A real number corresponding to the position of the axis, in millimetres. For example,
1237.222.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Velocity
Description
Queries the current speed of a motor.
Format
getVelocity_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getVelocity_1,1 returns the speed of the first motor connected to port 1.
Response
A real number corresponding to the speed of the axis, in mm/sec. For example,
400.12.
Positive numbers correspond to moving in the positive direction of the axis.
Negative numbers correspond to moving in the negative direction of the axis.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Target Reached
Description
Queries whether or not a motor has yet reached its target.
A motor is considered to have reached its target if any of these are satisfied:
it has reached its specified position or velocity for trapezoidal and continuous moves respectively
it has triggered one of its end of travel sensors
it has been interrupted by a quick stop command.
Format
getTargetReached_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getTargetReached_1,1 returns whether the first motor connected to port 1 has reached its target or not.
Response
0corresponds to the target not yet being reached.1corresponds to the target having been reached.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Motion Allowed
Description
Queries whether or not a motor is ready to accept new motion commands.
Generally, motion is allowed when target is reached or when operation is disabled.
Format
getMotionAllowed_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getMotionAllowed_1,1 returns whether the first motor connected to port 1 is ready to accept new motion commands or not.
Response
0corresponds to the motor not being ready to accept new motion commands.1corresponds to the motor being ready to accept new motion commands.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Brake Status
Description
Queries whether or not the brake is locked on a given motor.
Format
getBrakeStatus_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getBrakeStatus_1,1 returns whether the first motor connected to port 1 has its brake locked or not.
Response
0corresponds to the brake being unlocked.1corresponds to the brake being locked.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Home Sensor
Description
Queries whether or not the home sensor of a given motor is triggered.
Note: the conveyor motor does not have home nor end sensors. See “Get Sensor A” and “Get Sensor B” instead.
See MachineMotion AI Actuator Configuration End-of-travel sensors for more information on endstop sensors.
Format
getHomeSensor_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getHomeSensor_2,2 returns whether the second motor connected to port 2 has its home sensor triggered or not.
Response
0corresponds to the home sensor not being triggered.1corresponds to the home sensor being triggered.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get End Sensor
Description
Queries whether or not the endstop sensor of a given motor is triggered.
Note: the conveyor motor does not have home nor end sensors. See “Get Sensor A” and “Get Sensor B” instead.
See MachineMotion AI Actuator Configuration End-of-travel sensors for more information on endstop sensors.
Format
getEndSensor_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getEndSensor_2,1 returns whether the first motor connected to port 2 has its endstop sensor triggered or not.
Response
0corresponds to the endstop sensor not being triggered.1corresponds to the endstop sensor being triggered.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Sensor A
Compatibility
This command is available on MachineMotion software releases v3.4.0 and newer.
Description
Queries whether or not the sensor plugged into the port “A” of a given motor is triggered.
Note: This is especially useful for querying the state of conveyor motor sensors. For the step-servo motors, we recommend using rather “Get Home Sensor” and “Get End Sensor”.
See MachineMotion AI Actuator Configuration End-of-travel sensors for more information on endstop sensors.
Format
getSensorA_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getSensorA_2,1 returns whether the first motor connected to port 2 has the sensor plugged into port “A” triggered or not.
Response
0corresponds to the sensor not being triggered.1corresponds to the sensor being triggered.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Sensor B
Compatibility
This command is available on MachineMotion software releases v3.4.0 and newer.
Description
Queries whether or not the sensor plugged into the port “B” of a given motor is triggered.
Note: This is especially useful for querying the state of conveyor motor sensors. For the step-servo motors, we recommend using rather “Get Home Sensor” and “Get End Sensor”.
See MachineMotion AI Actuator Configuration End-of-travel sensors for more information on endstop sensors.
Format
getSensorB_<Payload>
Where <Payload> corresponds to <port>, <index> :
<port>is the motor address (port)<index>is the motor address (index)
Usage
getSensorB_2,1 returns whether the first motor connected to port 2 has the sensor plugged into port “A” triggered or not.
Response
0corresponds to the sensor not being triggered.1corresponds to the sensor being triggered.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Digital Input
Description
Reads a digital input from a Digital IO Module or a Push Button Module.
Format
getDigitalInput_<Payload>
Where <Payload> corresponds to <port>, <module> :
<port>is the module’s address (port it is connected to)<module>is the module’s address (device ID)<input>is the input pin number to read on the module. This is an optional parameter.
Usage
getDigitalInput_1,2,0 returns the current value of the input pin 0 from the module having the device ID 2, connected to the Control port 1.
getDigitalInput_1,2 returns the current value of all the input pins of the module having the device ID 2, connected to the Control port 1.
Response
A pin can have a value of
0or1.The value of all the pins of the module will be represented as a byte. For example,
15corresponds to0b1111, meaning that all 4 input pins of the module currently have a value of1.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get Digital Output
Description
Reads a digital output from a Digital IO Module or a Power Switch Module.
Format
getDigitalOutput_<Payload>
Where <Payload> corresponds to <port>, <module> :
<port>is the module’s address (port it is connected to)<module>is the module’s address (device ID)<output>is the output pin number to read on the module. This is an optional parameter.
Usage
getDigitalOutput_1,2,0 returns the current value of the output pin 0 from the module having the device ID 2, connected to the Control port 1.
getDigitalOutput_1,2 returns the current value of all the output pins of the module having the device ID 2, connected to the Control port 1.
Response
A pin can have a value of
0or1.The value of all the pins of the module will be represented as a byte. For example,
15corresponds to0b1111, meaning that all 4 output pins of the module currently have a value of1.ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Set Digital Output
Description
Writes a digital output from a Digital IO Module or a Power Switch Module.
Format
setDigitalOutput_<Payload>
Where <Payload> corresponds to <port>, <module> :
<port>is the module’s address (port it is connected to)<module>is the module’s address (device ID)<output>is the output pin number to write on the module<value>is the value to write to the pin
Usage
setDigitalOutput_1,2,0,1 writes the value 1 to the output pin 0 of the module having the device ID 2, connected to the Control port 1.
Response
1corresponds to a success0corresponds to a failureERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get User Input
Description
Reads a the value of a retained mqtt topic on the MachineMotion corresponding to a custom user input.
Format
getUserInput_<inputName>
Where <inputName> corresponds to the mqtt topic name.
Usage
getUserInput_CUSTOMINPUT returns the retained message of the mqtt topic tsapi/userInput/CUSTOMINPUT .
Response
A String corresponding to retained message on the given mqtt topic.
ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Get User Output
Description
Reads a the value of a retained mqtt topic on the MachineMotion corresponding to a custom user output.
Format
getUserOutput_<outputName>
Where <outputName> corresponds to the mqtt topic name.
Usage
getUserOutput_CUSTOMOUTPUT returns the retained message of the mqtt topic tsapi/userOutput/CUSTOMOUTPUT .
Response
A String corresponding to retained message on the given mqtt topic.
ERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
Set User Output
Description
Writes a the value of a retained mqtt topic on the MachineMotion corresponding to a custom user output.
Format
setUserOutput_<outputName>,<outputValue>
Where:
<outputName>corresponds to the mqtt topic name<outputValue>corresponds to the mqtt message
Usage
setUserOutput_CUSTOMOUTPUT,CUSTOMMESSAGE writes the retained message CUSTOMMESSAGE on the mqtt topic tsapi/userOutput/CUSTOMOUTPUT .
Response
1corresponds to a success0corresponds to a failureERROR <#>corresponds to a failure, where<#>will be the number corresponding to the error.
List of error numbers
Error Number | Error Description |
|---|---|
2 | Motion server not found |
3 | Bad request |
4 | Cannot read value |
5 | Bad input value |
6 | Input value is out of range |
7 | Motor not connected |
8 | Missing input value |
98 | Endpoint not found |
99 | Unknown error |
Documentation for Previous Releases
TCP Socket API for MachineMotion AI
MachineMotion AI v3.0.0 : not supported
MachineMotion AI v3.1.0 :
Initial release.
MachineMotion AI v3.2.0 and newer :
Introduced a breaking change by adding an end of line character to every command.
Introduced the heartbeat mechanism as well.