Cabling

  • Updated on Mar 17, 2025
  • Published on Feb 28, 2025
Introduction This cable (CE-CA-049-1000) connects the Digital I/O v2 module ( CE-MD-001-0000__2 ) to any 3rd party device using this M12 A-Keyed 4-Pin Female to pigtail 1m cable. This cable has a diameter of 8mm. The cable (CE-CA-049-1000) is a bu...
  • Published on Feb 20, 2025
Introduction This cable (CE-CA-110-4500) can be used to connect a Vention motor to a PLC or alternative controller by flying leads. Pinout
  • Published on Feb 28, 2025
The pin-out below is for CE-CA-105-2000 & CE-CA-106-2000 and applies to MachineMotion 2.