Documentation Index

Fetch the complete documentation index at: https://docs.vention.io/llms.txt

Use this file to discover all available pages before exploring further.

CAD File Import

Prev Next

This guide explains how to import custom components into MachineBuilder for use in your designs.

Feature Overview

Importing components into MachineBuilder allows users to design with custom parts, which behave like standard Vention components and work with all shortcuts. However, imported components:

  • Do not appear in the Bill of Materials (BOM).

  • Are not provided by Vention upon purchase of a design.

Supported File Types: .step, .stp, .sldprt, .stl, .iges, .igs, .prt, .catpart, .asm, .par, .ipt, .x_b, .x_t

Steps to Import a CAD File

Step 1: Select Your CAD Model

  1. Open the Import Window:

    • Option 1: From the menu in the top-left corner of the navigation bar, select CAD File Import.

    • Option 2: Navigate to the My Models section of the parts library and click Import Parts.

  2. Upload Your File:

    • Click Select Your File or drag and drop your file into the import window.

    • After selecting your file, switch to the Add Connectors tab to proceed.

Step 2: Add Connection Points (Optional)

  1. Add Connectors:

    • Click the Add Connector icon and attach it to the desired location on your imported model. This allows the model to snap to your Vention assembly.

    • Add as many connectors as needed.

  2. Edit Connectors:

    • Use the arrow keys to cycle through connectors for adjustments or deletion.

  3. Proceed to Properties:

    • Once the connectors are added, click Next to switch to the Edit Properties tab.

Step 3: Edit Properties

  1. Name Your Part:

    • Provide a descriptive name for easy identification in the My Models library.

  2. Input Optional Details:

    • Weight: Contributes to the overall design weight.

    • Assembly Time: Reflects in the design’s total assembly time.

    • Privacy Settings: Choose between personal visibility or sharing with your team on Vention’s platform.

    • Description: Add optional details about the part.

  3. Complete the Import:

    • Click Import to finalize the process. Your model will now behave like a standard Vention part in MachineBuilder.

Accessing Imported Models

All imported models can be found under the My Models section of the parts library, ready for use in your designs.