Deploy your Configuration and Applications to a MachineMotion

Prev Next

Introduction

This guide provides instructions for deploying a configuration and MachineLogic applications to a MachineMotion controller.

This document covers requirements for current version of MachineMotion controller. For previous version, refer to link below:

Documentation for Previous Product Versions

Setting up your MachineMotion Controller

Before proceeding, we recommend:

  • reviewing the MachineMotion: User Manual to familiarize yourself with the different methods of interfacing with the controller (e.g., using a computer or the Teach Pendant).

  • making sure you have followed the correct machine deployment steps here.

Using macOS

Since macOS Ventura, Apple has added network privacy control per app. Each app (including the Chrome web browser) must have explicit permission to access devices on the local network. Go to “System Settings > Privacy & Security > Local Network”, and ensure the permission is enabled.

From this point, you have two options for deploying your configuration and applications:

IMPORTANT NOTE: The servo-motors may lose power while the configuration gets applied, which engages the brakes. It is especially important for brakes to be installed on vertically positioned actuators.


Assisted Deployment Using MachineCloud

This section describes the steps required to establish a MachineCloud connection to your MachineMotion and deploy configuration and applications.

You can use MachineCloud in two ways, with or without providing Internet access to the MachineMotion:

  • via Internet:

    • You will first need to ensure that the MachineMotion is connected to the Internet.

    • You will need to use the exact MachineBuilder design that you purchased, as it is the one linked to your MachineMotion serial number.

  • via Ethernet:

    • This method does not require the MachineMotion to be connected to the Internet. Instead, you will need an Ethernet cable between your laptop and the “To PC” port of the MachineMotion.

    • You can use any MachineBuilder design.

Establishing Connection to MachineMotion

  1. From the MachineMotion’s Control Center:

    1. OPTIONAL - Ensure that your MachineMotion is connected to the internet:
      You can skip this step if you plan on using MachineCloud via Ethernet.
      Navigate to the “Settings“ page via the top navigation bar.
      Go to the Network section.
      Verify the presence of a blue “Access to Internet“ label.

    2. Ensure that no application is currently running:
      If the status of your MachineMotion is “Running”, you will need to stop the execution of any running application.
      To do so, you can navigate to the “Application Launcher” page via the top navigation bar.
      Then, click the Stop button to stop any running application.

    3. Enable Remote Access:
      In the top navigation bar, click or tap on the Cloud icon.
      Turn the “Remote Access” toggle on.
      Upon success, you should see the Remote Access screen.

      Figure 1 - ControlCenter Remote Access Screen

  2. From your web browser:

    1. Log in to your vention.io account, and open the design you have purchased.

      Note: Only purchased designs can be deployed using this method.

    2. Go to the MachineLogic tab.

    3. Click the “Deploy via MachineCloud“ dropdown.

    4. Depending on the method you want to use:

      1. via Internet: ensure the selected serial number matches the serial number displayed on the nameplate on the bottom of your MachineMotion.

      2. via Ethernet: select the “Ethernet via To PC” radio button

    5. The state of your MachineMotion will be displayed in the dropdown menu. The following table describes each possible state:

State

Description

Offline

The machine is currently offline. Ensure the MachineMotion is ON and connected to the internet.

Idle

The machine is not running any application and is ready for deployments.

Running

The machine is currently running an application and cannot accept new deployments.

Emergency Stop

The machine is currently in Emergency Stop mode. It is nevertheless ready for deployments.

Figure 2 - Deploy via MachineCloud dropdown

Deploying Configuration and Applications

Once connected to your machine, you can deploy your configuration and MachineLogic applications.
The types of data that can be deployed via MachineCloud are:

Payload Type

Description

Configuration

Represents the configuration of your machine, as defined in the Configuration tab, in the right pane of your design.

Design-level Scene Assets

These are scene assets defined in the Scene Assets tab, in the right pane of your design.
Design-level Scene Assets can be used by all MachineLogic applications.
Note: Application-level Scene Assets are automatically deployed with the application itself.

Code-Free applications

MachineLogic applications created using the Code-Free editor.

Python applications

MachineLogic applications created using the Python editor.

  1. From your web browser:

    1. Click the “Deploy via MachineCloud” dropdown.

    2. Select the items you wish to deploy.

    3. After making your selection, click the Deploy button at the bottom.

  2. From the Control Center:

    1. Once your deployment is complete, turn off the “Remote Access” mode, by clicking the toggle.

    2. In order to make use of your newly deployed assets, you will need to refresh the Control Center.
      You can do so by clicking the “Refresh” arrow of the navigation bar, at the top right of the screen.


Manual Deployment

Manual deployment is an alternative to the assisted deployment flow. It can be useful when you do not have the possibility of connecting your MachineMotion to the Internet. Follow these steps for successful deployment:

  1. From your web browser:

    1. Log in to your vention.io account, and open your design.

    2. Download your configuration file
      In the Configuration tab in the right pane, click “Download configuration”.
      You should have downloaded a .json file.

Figure 3 - Download the Configuration file

c. Download the MachineLogic applications
Click on the MachineLogic tab.
Open the application of your choice, and click “Download”.
You should have downloaded a .json file.
Repeat this step for each application you would like to deploy.

Figure 4 - Download the MachineLogic Application file

  1. From the Control Center:
    If you are using the Teach Pendant, you will need to plug in a USB key containing the files downloaded at step 1, in the back of the Teach Pendant.

    1. Upload the Configuration:
      Navigate to the Control Center “Settings” page via the top navigation bar.
      Click “Upload Configuration”.
      Select the configuration file you previously downloaded at step 1.

      Figure 4 - Control Center Settings page

    2. Upload the MachineLogic applications:
      Navigate to the “MachineLogic” page via the top navigation bar.
      Click “Upload App”.
      Select the application file(s) you previously downloaded at step 1.

      You can now play your applications via the “MachineLogic” page, or the “Application Launcher” page.

    If your application contains robot a scene assets, we recommend using the Calibration application.

    See the Calibration Application documentation.

Figure 5 - Control Center MachineLogic landing page, first option to upload applications

Figure 6 - Control Center MachineLogic application page, second option to upload applications

Documentation for Previous Product Versions