Robot Safety Module AI Datasheet

Prev Next

Overview

The Robot Safety Module AI CE-SA-016-0001__2 is intended to interface a robot with the MachineMotion AI. A change in the robot’s safety state (such as an emergency stop, a protective stop, or transitioning to collaborative mode) is propagated to the MachineMotion AI, and vice-versa. A dedicated port (Reduced Speed) can accomodate one or several safety modules, such as the Auto-Reset Module AI CE-SA-019-0001__2, in order to trigger the robot’s collaborative mode with light curtains or area scanners. The Robot Safety Module AI connects directly to the MachineMotion AI on the Robot port.

This document covers requirements for latest version of Vention’s Robot Safety Module. For previous version, refer to link below:

Documentation for Previous Product Versions

Features

  • Compatible with every model of MachineMotion AI

  • Compatible with most robot brands

  • Configuration-free: plug & play

  • Support for robot collaborative mode (reduced speed)

  • RGB LED indicator for safety status (emergency stop, collaborative mode, faults)

  • Single-color LED indicators for power and communication status

  • Publishes robot’s safety state to MachineMotion AI

  • Propagates MachineMotion AI’s safety state to the robot

Included cables

  • 1x Safety Extension cable - CE-CA-102-5000__3

  • 1x Robot Safety Module “TO ROBOT” cable - CE-SA-111-2550__2

  • 1x MachineMotion 2 Safety IN Pigtail cable - CE-CA-105-2000__2

  • 1x Safety Jumper - CE-SA-102-0001

Safety


Vention’s safety modules perform safety functions as a part of a whole installation or machine. A complete safety system normally includes sensors or input units, logic units and contactors or output units. The manufacturer of the installation or machine is responsible for ensuring proper functioning of the whole system. The total concept of the control system into which the safety module is integrated must be validated by the user. Vention cannot guarantee all specifications of an installation or a machine without being responsible for the risk assessment and the design of the safety system. Vention takes over no liability for recommendations which are given or implied in the following description.
The following items must be taken into consideration during the design, risk assessment & installation of the safety system :

  • The Safety Modules shall be put into operation only after the safety functions have been tested during the commissioning.

  • According to EN IEC 60204-1:2018 and EN ISO 10218-1:2011 it is not allowed to restart automatically after emergency stop. Therefore the control systems of the connected devices have to disable the automatic start after emergency stop.

  • Opening the Safety Module or implementing unauthorized changes voids any warranty.


Functional error! Danger to life, risk of serious injuries or property damage

  • The Robot Safety Module may only be used in VENTION safety ecosystem;

  • The Robot Safety Module should be connected to the MachineMotion AI’s Robots port;

  • The Robot Safety Module shall be connected to a robot according to its specific wiring diagram.

  • No emergency stop button shall be connected to the Safety IN port;

  • No emergency stop button shall be connected to the safety chain of the Reduced port;

  • The Robot Safety Module does not monitor the input redundant signals at the From Robot port. If the connected devices do not have monitoring of its output signals, the performance level of the safety function can be reduced;

  • If the robot is placed in reduced (collaborative mode) with a cycle time of less than 500s, the performance level may drop to PL d.

  • The Robot Safety Module is designed to operate in indoor environments without dust or high humidity. Dust and dampness may lead to malfunction. Do not install or operate the Safety Module outdoors;

Technical specs

General Specifications

Item

Specification

Part Number

CE-SA-016-0001__2

Weight

0.8kg

Dimensions

19.0 x 15.0 x 9.0mm

Material

  • Bottom enclosure: Aluminum

  • Top enclosure: Aluminum

Operating Temp

0 to 40°C

IP rating (IEC 60529)

IP54

Electrical Specifications

Item

Specification

Nominal input voltage

24 VDC (Class 2 or SELV power supply)*

Input voltage range

19.2 ~ 26.4 VDC

Max operating power consumption

8 W (with robot and MMAI operational)

Short circuit protection

Internal electronic fuse, max 2.5A

  • Note: In North America the Safety Module shall be supplied by a certified class 2 power supply. In Europe, the Safety Module must be supplied by an SELV circuit. When powered by the MachineMotion AI those requirements are met.

Physical Interface

Figure 1: Physical Interface

Figure 1: Physical Interface

LED Indicators

Name

LED Color

Indicates (when ON)

POWER

White

Power supplied to module

COMM

White

Ethernet communication functional

FUSE

Red

Module internal fuse tripped

STATUS

Off

Module disconnected

STATUS

Green

System operational

STATUS

Orange

Error

STATUS

Red

System emergency stop (not induced by robot)

STATUS

Blinking Red

Emergency stop induced by robot

STATUS

Blinking Blue

Collaborative mode (reduced speed)

Functionality

The Robot Safety Module AI is an easy way to interface almost any robot brand with a MachineMotion AI and other safety equipments. By properly wiring the module to the robot controller, the following safety behaviors will be achieved:

  • When the MachineMotion AI goes into emergency stop, the robot will go into emergency stop too.

  • When the robot goes into emergency stop (either from a protective stop or from the robot controller pendant e-stop button), the MachineMotion AI will go into emergency stop too.

  • When a user manages to reset the safety system, both the MachineMotion AI and the robot will go out of emergency stop simultaneously.

  • When a user attempts to reset the safety system but some faults have not been cleared, both the MachineMotion AI and the robot will stay in emergency stop.

  • When the devices connected to the Reduced Speed port are triggered, the robot will go into collaborative mode and the MachineMotion AI will be notified.

The collaborative mode is optional (see wiring diagrams). It can be implemented if, during an intervention by an individual, a safety function (other than emergency stop) needs to be enabled, such as a speed or force limitation.

No module with an e-stop button, such as the E-stop Reset Module (CE-SA-007-0000) and the E-stop Module (CE-SA-013-0000), should be connected to the Reduced Speed port.

The Robot Safety Module AI includes a 5-port Ethernet switch that connects the robot to the MachineMotion AI, alongside with every module daisychained to other ports (such as Reduced Speed). It also includes a microcontroller that controls the LED indicators and provides internal status reporting over Ethernet. Ethernet devices connected on any of the 4 safety ports of MachineMotion AI belong to the 192.168.5.0/24 subnet.

192.168.5.0/24

Reserved or Available

192.168.5.1

Reserved for Vention Pendant (static)

192.168.5.2

Reserved for MachineMotion AI (static)

192.168.5.3

Reserved for robot (static)

192.168.5.4 - 192.168.5.254

Available, can be assigned dynamically by MachineMotion AI (DHCP)

Port definitions and pinouts

Safety Out - M12, male, 12-pin, A-Keyed

The Safety Out port connects directly to the Robot port of the MachineMotion AI.

Pin

Function

Pin 1

24V input

Pin 2

0V input

Pin 3

OSSD output A (to MMAI)

Pin 4

OSSD input A (from MMAI)

Pin 5

OSSD output B (to MMAI)

Pin 6

OSSD input B (from MMAI)

Pin 7

Reset input

Pin 8

NC

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

Safety In - M12, female, 12-pin, A-Keyed

The Safety In port must normally be plugged with a yellow safety jumper CE-SA-102-0001 (included with MMAI).

Pin

Function

Pin 1

24V output

Pin 2

0V output

Pin 3

OSSD input A

Pin 4

OSSD output A

Pin 5

OSSD input B

Pin 6

OSSD output B

Pin 7

Reset output

Pin 8

NC

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

To Robot - M12, male, 12-pin, A-Keyed

Pin

Function

Pin 1

NC

Pin 2

NC

Pin 3

STO to Robot dry contact output 1-1

Pin 4

STO to Robot dry contact output 1-2

Pin 5

STO to Robot dry contact output 2-1

Pin 6

STO to Robot dry contact output 2-2

Pin 7

NC

Pin 8

Reset output

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

From Robot - M12, female, 12-pin, A-Keyed

Pin

Function

Pin 1

Robot STO input 1

Pin 2

Robot STO input 2

Pin 3

NC

Pin 4

NC

Pin 5

0V

Pin 6

Collaborative mode dry contact output 1-1

Pin 7

Collaborative mode dry contact output 1-2

Pin 8

Collaborative mode dry contact output 2-1

Pin 9

Collaborative mode dry contact output 2-2

Pin 10

NC

Pin 11

NC

Pin 12

NC

Reduced Speed - M12, female, 12-pin, A-Keyed

Pin

Function

Pin 1

24V output

Pin 2

0V output

Pin 3

OSSD input A

Pin 4

24 VDC output

Pin 5

OSSD input B

Pin 6

24 VDC output

Pin 7

Reset output

Pin 8

0V output

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

Mounting

Install the module mounting bracket (CE-HW-005-1002) to the extrusion with the screws provided (HW-FN-003-0018). Install the module onto the mounting bracket as illustrated below.

Figure 3: Module Mounting

Figure 3: Module Mounting

Figure 3: Module Mounting

Figure 3: Module Mounting

Wiring Diagrams with MachineMotion

Figure 4: Robot Safety Module wiring diagram

Figure 5: Robot Safety Module wiring diagram with Mode Switching Module (CE-SA-018-0001__2)

Diagram showing components of a robotic safety system with labeled connections and modules.

Figure 6: Robot Safety Module wiring diagram with Auto-Reset Module (CE-SA-019-0001__2)

*Note: Insert a jumper on any unused safety input for proper functionality. See table below to identify the appropriate jumper part number (included with the module).

Jumper Part Number

Description

Target module

Port restrictions

CE-SA-125-0001

M12, male, 12 pins, black jumper

Muting Safety Module AI (CE-SA-015-0001__2)
Mode Switching Module AI (CE-SA-018-0001__2)
Auto-Reset Module AI (CE-SA-019-0001__2)

Strictly reserved for Device ports

CE-JP-000-0002

M12, male, 4 pins, yellow jumper

Access Request Module AI (CE-SA-017-0001__2)

Strictly reserved for End Effector port

CE-SA-102-0001

M12, male, 12 pins, yellow jumper

All modules

Other unused safety input ports

Robot Wiring & Configuration

For instructions on how to wire & configure your robot controller please see the documents below:

Important information

  • No module with an emergency stop button should ever be placed on the Reduced Speed port.

  • The electronic fuse contained in the Robot Safety Module AI only protects from internal faults. 24V power outputs on the Safety In and Reduced Speed ports are not protected by the electronic fuse. The electronic fuse has an auto-retry mechanism (it does not latch faults and does not require a power cycle to reset).

Safety Data

The Robot Safety Module realizes the following safety functions :

  • System emergency stop output at the Safety OUT port from the Safety IN port (Estop_SafetyIN-to-SafetyOUT);

  • System emergency stop output at the To Robot port from the Safety IN port (Estop_SafetyIN-to-Robot);

  • System emergency stop output at the Safety OUT port from the From Robot port (Estop_FromRobot);

  • Redundant safe signal at the From Robot port from the Reduced port (Reduced_FromRobot);

  • System reset propagation from the Safety IN port to the Safety OUT port (Reset_SafetyOUT); and

  • System reset propagation from the Safety IN port to the To Robot port (Reset_ToRobot).

For each of these functions, safety data can be found in the following table.

Safety Function

PL

Cat.

MTTFd

DCavg

PFHd

Response time

E-stop_SafetyIN-to-SafetyOUT

e

3

224

99%

4.29E-08

20 ms

Estop_SafetyIN-to-Robot

e

3

186

99%

4.29E-08

30 ms

Estop_FromRobot

e

3

224

99%

4.29E-08

20 ms

Reduced_FromRobot

e

3

186

99%

4.29E-08

20 ms

Reset_SafetyOUT

c

1

>100

N/A

1.14E-06

Not applicable

Reset_ToRobot

c

1

>100

N/A

1.14E-06

Not applicable

The above information have been calculated based on the following operation conditions:

Data

Value

Unit

dop

365

days/years

hop

24

hours/days

tcycle

8640

s/cycle

If the robot is placed in reduced (collaborative mode) with a cycle time of less than 500s, the performance level may drop to PL d.

Documentation for Previous Product Versions