Documentation Index

Fetch the complete documentation index at: https://docs.vention.io/llms.txt

Use this file to discover all available pages before exploring further.

Custom HMI Development

Prev Next

We now provide a starter template with all the code necessary to run, display, and automatically rebuild a React application when changes are detected.

Quick Start - Hello World Example

The simplest possible UI application consists of an index.html file in the ui/ folder with plain HTML, CSS, and JavaScript — no build step required.

1- Inside a new Python application, create a new directory and give it the name ui

2- In the new ui directory, create a new file and name it index.html

3- open the index.html file and paste this snippet:

<!doctype html>
<html lang="en">
  <head>
    <meta charset="UTF-8" />
    <meta name="viewport" content="width=device-width, initial-scale=1.0" />
    <title>My HMI</title>
    <style>
          button { font-size: 100px }
    </style>
  </head>
  <body>
    <div id="root">
      
      <button id="mybutton" onclick="ThisIsAButton()">
        This is a Button! 
      </button>
    </div>
    <script>
      function ThisIsAButton() {
        alert("Hello World!")
      }
    </script>
  </body>
</html>

4- to see the Custom UI in action, select the Open HMI button. you will see the content of the index.html rendered in our HMI visualizer:

Simple Custom HMI example

Getting Started

Option 1: Using the Application Template (Recommended)

Simply select PythonTemplate in the Machine Logic New Application dropdown. This will provide you with everything you need to start developing your custom UI application.

Accessing the application template


Option 2: Local Development Setup

If you decide to start your frontend application locally instead, you'll need to ensure your project configuration matches the required specifications.

Step 1: Configure package.json

Your package.json must have versions that match the demo, in particular for Vite and React:

{
  "name": "your-custom-ui-app",
  "version": "1.0.0",
  "type": "module",
  "scripts": {
    "dev": "vite",
    "build": "vite build",
    "preview": "vite preview"
  },
  "dependencies": {
    "@emotion/react": "11.13.3",
    "@emotion/styled": "11.13.0",
    "@mui/icons-material": "5.16.7",
    "@mui/material": "5.16.7",
    "@mui/styles": "5.16.7",
    "@tabler/icons-react": "3.35.0",
    "@vention/machine-logic-ui-sdk": "0.27.3",
    "@vention/machine-ui": "3.38.0",
    "@vention/machine-apps-components": "0.3.22",
    "buffer": "6.0.3",
    "dayjs": "1.11.18",
    "react": "17.0.2",
    "react-dom": "17.0.2",
    "react-draggable": "4.4.6",
    "react-hook-form": "7.53.0",
    "react-router-dom": "6.26.2",
    "tss-react": "4.9.13"
  },
  "devDependencies": {
    "@types/node": "^20.10.0",
    "@types/react": "17.0.82",
    "@types/react-dom": "17.0.25",
    "@vitejs/plugin-react": "^4.3.4",
    "typescript": "5.4.5",
    "vite": "^6.0.0"
  },
  "engines": {
    "node": ">=20",
    "npm": ">=8"
  }
}

Critical versions to match:

  • React: 17.0.2

  • Vite: ^6.0.0

  • TypeScript: 5.4.5

Step 2: Configure vite.config.ts

Create a vite.config.ts with the following configuration:

import { defineConfig } from "vite"
import react from "@vitejs/plugin-react"
import path from "path"
export default defineConfig({
  plugins: [react()],
  base: "./",
  resolve: {
    alias: {
      "@": path.resolve(__dirname, "./src"),
    },
  },
  build: {
    outDir: "../ui",
    emptyOutDir: true,
    minify: "esbuild",
    target: "esnext",
    cssMinify: "esbuild",
    sourcemap: false,
  },
  server: {
    port: 5173,
    host: true,
    hmr: {
      overlay: true,
    },
  },
  optimizeDeps: {
    include: ["react", "react-dom", "@mui/material", "@emotion/react", "@emotion/styled"],
  },
})

Key configuration points:

  • base: "./" - Uses relative paths for assets (required for proper loading)

  • outDir: "../ui" - Outputs build to the ui folder at the parent level

  • target: "esnext" - Modern JavaScript output


Autobuild Feature Requirements

To enable the automatic rebuild feature, your project must follow this folder structure:

Required Folder Structure

your-application/
├── customui/          ← Your react source code goes here
│   ├── src/
│   │   └── main.tsx
│   ├── index.html
│   ├── package.json
│   ├── vite.config.ts
│   └── tsconfig.json
└── ui/                ← Build output goes here (auto-generated)
    ├── index.html
    └── assets/
        ├── main.js
        └── main.css

Build Output Requirements

Your build script must output the built files to a ui folder at the same level as the customui folder. With the vite.config.ts provided above, running vite build will automatically output to ../ui, which satisfies this requirement.


Summary

Requirement

Details

Source folder

customui/

Build output folder

ui/ (same level as customui)

React version

17.0.2

Vite version

^6.0.0

Node.js

>=20

npm

>=8

Build base path

"./" (relative)

Target

esnext

For the quickest setup, use the Application Template option in Machine Logic. For custom local development, ensure all configurations match the specifications above.


Advanced: Faster Build with esbuild

The Application Template includes an optimized build script using esbuild directly, which is faster than the standard Vite build. If you want to use this approach, update your package.json with the following:

{
  "scripts": {
    "dev": "vite",
    "build": "esbuild src/main.tsx --bundle --outdir=../ui/assets --format=esm --target=esnext --loader:.tsx=tsx --loader:.ts=ts --loader:.css=css --splitting --entry-names=main --chunk-names=[name]-[hash] && sed 's|/src/main.tsx|./assets/main.js|g' index.html | sed 's|</head>|<link rel=\"stylesheet\" href=\"./assets/main.css\"></head>|g' > ../ui/index.html && chmod -R g+w ../ui",
    "preview": "vite preview"
  },
  "devDependencies": {
    "esbuild": "^0.24.0"
  }
}

Build Script Breakdown

This script performs the following steps:

# 1. Bundle with esbuild
esbuild src/main.tsx --bundle --outdir=../ui/assets \
  --format=esm --target=esnext \
  --loader:.tsx=tsx --loader:.ts=ts --loader:.css=css \
  --splitting --entry-names=main --chunk-names=[name]-[hash]
# 2. Transform index.html and output to ui folder
sed 's|/src/main.tsx|./assets/main.js|g' index.html | \
sed 's|</head>|<link rel="stylesheet" href="./assets/main.css"></head>|g' \
> ../ui/index.html
# 3. Set group write permissions
chmod -R g+w ../ui

What each part does:

  1. esbuild bundling - Compiles and bundles the TypeScript/React code with code splitting enabled

  2. HTML transformation - Updates index.html to reference the built assets:    

    • Replaces /src/main.tsx with ./assets/main.js

    • Adds the CSS stylesheet link to the head

  3. Permissions - Sets group write permissions on the output folder

This approach is faster for incremental rebuilds but requires the additional sed commands to transform the HTML file.