This starter template helps you build machine applications — apps that control or monitor Vention-powered automation systems.
It comes with everything you need to get started quickly:
- 🧠A Python backend that defines how your machine behaves
- 💾 A database layer that remembers configurations and results
- 💻 A React frontend that operators interact with
It uses three key tools from the Vention Developer Toolkit:
- Vention Storage — Saves and tracks your app’s data
- Vention State Machine — Controls the application logic
- Machine UI — Low level Vention-styled UI components
Table of Contents
- Overview
- Project Structure
- Backend Files
- Frontend Files
- Key Features Demonstrated
- Demo Application: Multiplication Quiz
- Notes
Overview
This starter template provides a complete example of building modern machine applications using the Vention developer toolkit. It includes:
- State Machine: Real-time demo application using
vention-state-machine - Data Storage: Persistent storage with audit trails using
vention-storage - React Frontend: Modern UI using
@ventionco/machine-uiand@ventionco/machine-apps-componentsassets
Project Structure
machine-code-demo/
├── customui/ # React frontend source code
│ └── src/
│ ├── app/ # Main application components
│ │ ├── pages/ # Page components
│ │ ├── api.ts # Type-safe API client
│ │ ├── app-context.tsx # React context for state management
│ │ └── app.tsx # Main app component and router
│ └── main.tsx # Application entry point
├── app.py # State machine implementation
├── models.py # Data models
├── requirements.txt # Python dependencies
├── server.py # FastAPI server
└── [build config files]
Backend Files
app.py
Core state machine implementation using vention-state-machine. This file contains:
- Robot Reach Study State Machine: Three-state workflow (generating → presenting → grading)
- Automatic Timeouts: Configurable timeout handling with countdown timers
- Guard Conditions: Answer validation before state transitions
models.py
Data models using SQLModel for vention-storage integration:
- Quiz Model: Stores multiplication problems and user answers
- Configuration Model: Runtime settings for configuring the quiz
- Automatic Validation: Built-in answer correctness calculation
server.py
FastAPI server that provides:
- Automatic CRUD APIs: Generated REST endpoints for all models
- Audit Trails: All operations tracked with user attribution
- Bootstrap Integration: One-command setup with
vention-storage
requirements.txt
Python dependencies including:
fastapi- Modern web frameworkuvicorn- ASGI servervention-state-machine- State machine libraryvention-storage- Data persistence with audit trailssqlmodel- Type-safe database models
Frontend Files
customui/src/app/app.tsx
Main application page, contains:
- Status Indicator and Robot Controls: Leveraging
@ventionco/machine-app-components - Routing: React router for the quiz and settings pages
customui/src/app/api.ts
API helpers for communicating with the backend:
- Types: Request/Response models for all endpoints
- REST endpoints: Strongly typed REST calls using
fetch
customui/src/app/app-context.tsx
React context provider:
- Hooks: Provide granular access to specific parts of the context
- Callbacks: Memo wrapper around the API calls
- Data Store: Remember the latest state/quiz from the backend
customui/src/app/pages/
The individual pages:
- operation-page.tsx: The reach study quiz itself, triggers transitions in the state machine
- settings-page.tsx: The app configuration page, reads/writes to the database through the storage module
Key Features Demonstrated
This starter template showcases:
- Modern State Management: Using
vention-state-machinefor complex application workflows - Persistent Data Storage: Using
vention-storagewith automatic CRUD APIs and audit trails - Type Safety: Front-to-back strong typing with complete openAPI spec
- Modern UI: React with Material-UI components and responsive design
- Development Experience: Hot reload, auto-reload, and comprehensive API documentation
Demo Application: Multiplication Quiz
This starter template includes a complete demo application that showcases how to build a real-time, state-driven application using the Vention developer toolkit libraries. The demo is a multiplication quiz that demonstrates best practices for:
- State Management: Using
vention-state-machinefor complex application workflows - Data Persistence: Using
vention-storagefor robust data management with audit trails - Modern UI: React frontend with Material-UI components
How Vention Libraries Are Used
🎯 Vention State Machine (vention-state-machine)
The demo showcases a sophisticated state machine with three main states:
class QuizStates(StateGroup):
generating: State = State() # Creating new problems
presenting: State = State() # Displaying problems to user
grading: State = State() # Waiting for user input
Key Features Demonstrated:
- Declarative State Definition: Using
StateGroupandStateclasses for type-safe state management - Automatic Timeouts: Problems auto-fault if not answered within the timeout period
- Guard Conditions: Only correct answers can trigger state transitions
- Lifecycle Hooks: State entry/exit callbacks for UI updates and countdown timers
State Flow:
generating→ Creates new multiplication problem (1s delay)presenting→ Displays problem to user (immediate transition)grading→ Waits for user answer with countdown timerfault→ Entered if timeout expires (auto-recovery via reset)
💾 Vention Storage (vention-storage)
The demo uses vention-storage for robust data management with automatic audit trails:
Data Models:
class Quiz(SQLModel, table=True):
id: Optional[int] = Field(default=None, primary_key=True)
first_number: int
second_number: int
solution: Optional[int] = None # User-provided answer
correct: Optional[bool] = None # Auto-evaluated correctness
class Configuration(SQLModel, table=True):
id: Optional[int] = Field(default=None, primary_key=True)
max_number: int = Field(default=12) # Max operand value
timeout_seconds: int = Field(default=10) # Answer timeout
Key Features Demonstrated:
- Automatic CRUD API: Full REST endpoints generated automatically (
/quiz/,/config/) - Audit Trails: All data changes tracked with actor attribution (
X-Userheader) - Lifecycle Hooks: Before-update validation to auto-calculate correct answers
- Bootstrap System: One-command setup with
bootstrap()function - Type Safety: Full TypeScript integration with generated API types
Storage Operations:
- Quiz Creation: New problems automatically inserted with audit trail
- Answer Validation: Solutions validated against correct answer with automatic
correctfield update - Configuration Management: Runtime settings stored and retrieved via REST API
- Audit Logging: All operations tracked with timestamps and user attribution
Demo Workflow
- Startup: State machine begins in
readystate, configuration loaded from storage - Problem Generation: User triggers
start→generatingstate → creates new quiz problem - Problem Presentation: Auto-transitions to
presenting→ displays problem to user - Answer Collection: Enters
gradingstate → starts countdown timer → waits for user input - Answer Validation: User submits answer → stored in database → validated against correct solution
- State Transition: If correct → returns to
generatingfor next problem; if timeout → entersfault - Recovery: User can reset from
faultstate to continue
Real-time Features
- Progress Indicators: Visual countdown timer showing time remaining
- Error Handling: Graceful fault state with user-friendly recovery options
- Responsive UI: State-driven rendering with appropriate loading states and feedback
Configuration Options
The demo supports runtime configuration via the storage system:
- Maximum Number: Controls difficulty (operands from 1 to max_number)
- Timeout Seconds: How long users have to answer each problem
- Real-time Updates: Configuration changes immediately affect new problems
This demo serves as a comprehensive example of how to build production-ready applications using the Vention developer toolkit, showcasing both the power and simplicity of the state machine and storage libraries.
Notes
- The demo application runs independently and can be tested locally using
uvicorn backend.server:app --reload - The React UI will only be visible when accessing the HMI in the MachineLogic platform or locally
- The application uses SQLite for data persistence, which is automatically created on first run
- All data operations are automatically audited with timestamps and user attribution