Documentation Index

Fetch the complete documentation index at: https://docs.vention.io/llms.txt

Use this file to discover all available pages before exploring further.

State Machine

Prev Next

A lightweight wrapper around transitions for building async-safe, recoverable hierarchical state machines with minimal boilerplate.

Table of Contents

✨ Features

  • Built-in ready / fault states
  • Global transitions: to_fault, reset
  • Optional state recovery (recover__state)
  • Async task spawning and cancellation
  • Timeouts and auto-fault handling
  • Transition history recording with timestamps + durations
  • Guard conditions for blocking transitions
  • Global state change callbacks for logging/MQTT
  • Optional FastAPI router for HTTP access and visualization

🧠 Concepts & Overview

This library uses a declarative domain-specific language (DSL) to define state machines in a readable, strongly typed way.

  • State → A leaf node in the state machine
  • StateGroup → Groups related states, creating hierarchical namespaces
  • Trigger → Named events that initiate transitions

Example:

class MyStates(StateGroup):
    idle: State = State()
    working: State = State()

class Triggers:
    begin = Trigger("begin")
    finish = Trigger("finish")

TRANSITIONS = [
    Triggers.finish.transition(MyStates.working, MyStates.idle),
]

Base States and Triggers

All machines include:

States:

  • ready (initial)
  • fault (global error)

Triggers:

  • start, to_fault, reset
from state_machine.core import BaseStates, BaseTriggers

state_machine.trigger(BaseTriggers.RESET.value)
assert state_machine.state == BaseStates.READY.value

⚙️ Installation & Setup

pip install vention-state-machine

Optional dependencies:

  • Graphviz (required for diagram generation)
  • FastAPI (for HTTP exposure of state machine)

🚀 Quickstart Tutorial

1. Define States and Triggers

from state_machine.defs import StateGroup, State, Trigger

class Running(StateGroup):
    picking: State = State()
    placing: State = State()
    homing: State = State()

class States:
    running = Running()

class Triggers:
    start = Trigger("start")
    finished_picking = Trigger("finished_picking")
    finished_placing = Trigger("finished_placing")
    finished_homing = Trigger("finished_homing")
    to_fault = Trigger("to_fault")
    reset = Trigger("reset")

2. Define Transitions

TRANSITIONS = [
    Triggers.start.transition("ready", States.running.picking),
    Triggers.finished_picking.transition(States.running.picking, States.running.placing),
    Triggers.finished_placing.transition(States.running.placing, States.running.homing),
    Triggers.finished_homing.transition(States.running.homing, States.running.picking),
]

3. Implement Your State Machine

from state_machine.core import StateMachine
from state_machine.decorators import on_enter_state, auto_timeout, guard, on_state_change

class CustomMachine(StateMachine):
    def __init__(self):
        super().__init__(states=States, transitions=TRANSITIONS)

    @on_enter_state(States.running.picking)
    @auto_timeout(5.0, Triggers.to_fault)
    def enter_picking(self, _):
        print("🔹 Entering picking")

    @on_enter_state(States.running.placing)
    def enter_placing(self, _):
        print("🔸 Entering placing")

    @on_enter_state(States.running.homing)
    def enter_homing(self, _):
        print("🔺 Entering homing")

    @guard(Triggers.reset)
    def check_safety_conditions(self) -> bool:
        return not self.estop_pressed

    @on_state_change
    def publish_state_to_mqtt(self, old_state: str, new_state: str, trigger: str):
        mqtt_client.publish("machine/state", {
            "old_state": old_state,
            "new_state": new_state,
            "trigger": trigger
        })

4. Start It

state_machine = StateMachine()
state_machine.start()

🛠 How-to Guides

Expose Over HTTP with FastAPI

from fastapi import FastAPI
from state_machine.router import build_router
from state_machine.core import StateMachine

state_machine = StateMachine(...)
state_machine.start()

app = FastAPI()
app.include_router(build_router(state_machine))

Endpoints:

  • GET /state → Current state
  • GET /history → Transition history
  • POST /<trigger> → Trigger a transition
  • GET /diagram.svg → Graphviz diagram

Timeout Example

@auto_timeout(5.0, Triggers.to_fault)
def enter_state(self, _):
    ...

Recovery Example

state_machine = StateMachine(enable_last_state_recovery=True)
state_machine.start()  # will attempt recover__{last_state}

How-to: Run and Cancel Async Tasks

The state machine can manage background coroutines that should be cancelled automatically when a transition occurs (e.g. leaving a state or hitting fault).

import asyncio
from state_machine.core import StateMachine
from state_machine.defs import State, StateGroup, Trigger
from state_machine.decorators import on_enter_state

class MyStates(StateGroup):
    monitoring: State = State()

class States:
    monitoring = MyStates()

class Triggers:
    start = Trigger("start")
    to_fault = Trigger("to_fault")

TRANSITIONS = [
    Triggers.start.transition("ready", States.monitoring.monitoring),
]

class MonitoringMachine(StateMachine):
    def __init__(self):
        super().__init__(states=States, transitions=TRANSITIONS)

    @on_enter_state(States.monitoring.monitoring)
    def enter_monitoring(self, _):
        # Spawn an async background task (e.g. polling a sensor)
        async def poll_sensor():
            while True:
                print("🔎 Checking sensor...")
                await asyncio.sleep(1)

        self.spawn(poll_sensor())

The spawn() method wraps asyncio.create_task and tracks the task.

On a transition to fault (via to_fault) or any time cancel_tasks() is called, all tracked tasks are cancelled cleanly.

Manual cancellation example:

machine = MonitoringMachine()
machine.start()

# later in your app
await machine.cancel_tasks()

📖 API Reference

StateMachine

class StateMachine(HierarchicalGraphMachine):
    def __init__(
        self,
        states: Union[object, list[dict[str, Any]], None],
        *,
        transitions: Optional[list[dict[str, str]]] = None,
        history_size: Optional[int] = None,
        enable_last_state_recovery: bool = True,
        **kw: Any,
    )

Parameters:

  • states: Either a container of StateGroups or a list of state dicts.
  • transitions: List of transition dictionaries, or [].
  • history_size: Max number of entries in transition history (default 1000).
  • enable_last_state_recovery: If True, machine can resume from last recorded state.

Methods

spawn(coro: Coroutine) -> asyncio.Task
Start a background coroutine and track it. Auto-cancelled on fault/reset.

cancel_tasks() -> None
Cancel all tracked tasks and timeouts.

set_timeout(state_name: str, seconds: float, trigger_fn: Callable[[], str]) -> None
Schedule a trigger if state_name stays active too long.

record_last_state() -> None
Save current state for recovery.

get_last_state() -> Optional[str]
Return most recently recorded state.

start() -> None
Enter machine (recover__... if applicable, else start).

Properties

history -> list[dict[str, Any]]
Full transition history with timestamps/durations.

get_last_history_entries(n: int) -> list[dict[str, Any]]
Return last n transitions.

Decorators

@on_enter_state(state: State)
Bind function to run on entry.

@on_exit_state(state: State)
Bind function to run on exit.

@auto_timeout(seconds: float, trigger: Trigger)
Auto-trigger if timeout expires.

@guard(*triggers: Trigger)
Guard transition; blocks if function returns False.

@on_state_change
Global callback (old_state, new_state, trigger) fired after each transition.

Router

def build_router(
    machine: StateMachine,
    triggers: Optional[list[Trigger]] = None
) -> fastapi.APIRouter

Exposes endpoints:

  • GET /state
  • GET /history
  • POST /<trigger>
  • GET /diagram.svg

🔍 Troubleshooting & FAQ

  • Diagram endpoint returns 503 → Graphviz not installed.
  • Transitions blocked unexpectedly → Check guard conditions.
  • Callbacks not firing → Only successful transitions trigger them.
  • State not restored after restart → Ensure enable_last_state_recovery=True.