Small Gantry Enclosed Timing Belt Actuator

Prev Next

Overview

The small gantry enclosed timing belt is a high-performance actuator that opens new possibilities, with a pinch point-free design enabling work in dirty environments. This actuator incorporates a gantry with the same width as the extrusion housing to accommodate a wider range of space constrained applications.

Keep reading the following technical document to understand the detailed specifications of this actuator.

Cover image of technical document

Composition

The enclosed timing belt actuator is composed of the following parts:

  1. A thin spring-steel cover seals the top of this enclosed timing belt actuator, keeping contaminants out and eliminating pinch points. Note: Cover is not load-bearing. Do not apply a load to it, or it can break.

  2. A specially designed extrusion profile provides the outer structure and mounting points, in keeping with Vention’s extrusion ecosystem.

  3. An in-line gantry plate forms the actuator’s main mobile structure. Use it to attach components, like hardware or another actuator, that you would like to move around.

  4. A tensioner sets the tension of the 20 mm wide HTD8 belt using an M5 screw locked in place by a set screw.

  5. A single profile bearing carries loads and moments while ensuring smooth low-friction operation.

  6. The bearing rolls along the linear profile guide rail, which is made of hardened steel and attached to the extrusion body.

  7. The timing belt pulleys have full 180 degree belt engagement to ensure belt slip will not occur.

  8. A 20 mm wide HTD8 belt provides high-output force capacity, allowing the small-gantry timing belt actuator to be used for light or heavy loads  while maintaining  positional accuracy.

  9. Internal bump stops ensure that if the actuator impacts the end of travel no components will be damaged.

  10. Easy to access sensor ports for home and end of travel detection.

Applications

The small-gantry enclosed timing belt is a robust, compact actuator that can be used in horizontal and vertical configurations. Mount in any direction to suit your needs; its flexibility makes it suitable for a multitude of applications.

One great use for the small-gantry enclosed timing belt is for 2 or 3-axis gantry applications. These applications can be used for short-stroke pick and place, small-sized product inspection, engraving, routing, etc.

The benefit of having a gantry with the same width as the extrusion is the ability to mount these actuators very close together to minimize the space used for a given application.

3-Axis Gantry System

3-Axis Gantry System

2-Axis Gantry System

2-Axis Gantry System

Explore public designs to get ideas on how you could use the enclosed timing belt actuator.

Browse open-source designs

Technical Specifications

The table below lists the overall performance specs for the enclosed timing belt actuator. For details see sections Load Capacity, and Driving Force.

Displacement Ratio (mm/motor shaft rotation)

208

Force per unit of input torque (N / Nm)

30.2

Maximum input torque (Nm)

61

Repeatability including backlash (mm)

±0.3

Total Backlash (mm)

0.25

Backdrive Resistance

Low

Max Lifting Capacity

See Driving Force

Motor Compatibility

NEMA 34, 14mm shaft with 5mm key

Sensor Compatibility

CE-SN-004-0003 Flush Inductive Proximity Sensor

Load Capacity

The table below shows the load capacity of the three configurations of the small-gantry enclosed timing belt. Both nominal and max peak forces are specified in each direction. Use the diagram below to understand the directional load and moment capacities.

Nominal Axial Force (Fx)

See Driving Force

Max Peak Axial Force (Fx)

1240 N

Nominal Roll Moment (Mx)

100 Nm

Max Peak Roll Moment (Mx)*

255 Nm

Nominal Horizontal Force (Fy)

1200 N

Max Peak Horizontal Force (Fy)*

1800 N

Nominal Pitch Moment (My)

43.5 Nm

Max Peak Pitch Moment (My)*

115 Nm

Nominal Vertical Force (Fz)

1200 N

Max Peak Vertical Force (Fz)*

1800 N

Nominal Yaw Moment (Mz)

62 Nm

Max Peak Yaw Moment (Mz)*

115 Nm

The nominal values are valid for an actuator in motion with a rated lifespan of 2,000,000 cycles.

*Note that max peak values represent the absolute maximum load. Peak loads are acceptable during one-time events such as emergency stops, but operating at peak loads continuously will cause excessive wear and significantly decrease the actuator’s lifespan.

Driving Force

Output force indicates how much weight the actuator can move and how quickly it can accelerate that load. This force is shown as “Fx” in the Load Capacity figure. For a more in-depth explanation of driving force, see the section of our linear actuator selection guide that covers calculating actuator forces, or ask your application engineer for an explanation and help with calculations.

Graph showing the relationship between force and speed for a timing belt system.

The above graph shows the driving force of the enclosed axis and the range of achievable operational speeds (the linear range is the limiting factor). The three different curves represent the actuator’s performance with the three types of NEMA 34 motors offered by Vention.

Notes:

  • These performance curves are made with our motors and controller at steady state conditions. Using others motors or controllers will have different behavior therefore performance and reliability cannot be guaranteed.

  • Performance curves represent peak torque and speed values. Actual continuous performance may be lower due to I²t protection in the driver. For applications involving continuous, sustained torque output, contact Vention support for thermal derating guidelines or continuous-duty application advice.

  • Motors are equipped with an integrated safety mechanism known as I²T protection, which prevents overheating. This function continuously monitors the current drawn by the motor over time. If the motor operates at full load for an extended period (approximately 40–60 seconds), the I²T protection engages and limits the current, thereby reducing the available torque. The dashed lines in the graph illustrate the motor’s performance under these conditions. Once the motor has cooled sufficiently, it automatically returns to normal operating mode.

  • When two motors are mounted on the same actuator and operated in Cyclic Synchronous Torque (CST) mode, an increase in actuator output force of 1.8× can be expected. This performance gain is only applicable when both motors are synchronized in CST mode. Motors that are synchronized—but not operating in CST mode—do not yield this increase.

Assembly Instructions

Sensor Installation

The enclosed axis comes completely assembled. All you need to do is install your choice of powertrain components, such as brakes, gearbox, motor, and sensors.

Sensors can be installed in any of the four sensor port locations. To install a sensor, remove the port plug and screw the sensor all the way into the hole until it bottoms out. Install one jam nut and tighten it to lock the sensor in place.

Powertrain Installation

To connect powertrain components (stepper motor, brake and gearbox), perform the following steps:

  • Remove the motor cover on the actuator endblock, to install the stepper motor.

  • Optional: If you have a brake or gearbox, connect them to the output shaft of the stepper motor using the provided M6 X 20mm fasteners.

  • Connect your stepper motor to the actuator using x4 M6 X 20mm fasteners (HW-FN-005-0020).

Notes:

  • When installing motors, apply a small amount of grease to the motor shaft so that it is lightly coated. This will reduce the possibility of fretting corrosion occurring during operation, making future removal easier.

  • Moreover, do not use excessive force (hammering, prying or using screws to “push” the motor) to install the motor.

Mounting Features

Once the powertrain and sensors are in place, attach the actuator to your structure by connecting any appropriate structural component to the actuator’s gantry plate or end blocks.

When mounting multiple enclosed actuators in parallel, please refer to the self aligning mount technical document found here.

Maintenance

For maintenance instructions please refer to the appropriate section in our Maintenance Technical Document.