Documentation Index

Fetch the complete documentation index at: https://docs.vention.io/llms.txt

Use this file to discover all available pages before exploring further.

Mode Switching Safety Module AI Datasheet

Prev Next

Overview

The Mode Switching Safety Module AI (CE-SA-018-0001__2) is ideal for applications where partial body entry into a machine is necessary without triggering an emergency stop (e-stop). A typical example is an operator replacing a part during machine tending. At each cycle, the machine’s automation program pauses for the time required by the operator to replace the part. A safe sensor (device A) detects the end of a cycle and mutes a light curtain (device B) for a few seconds until the operator completes the replacement. The program then resumes and the next cycle proceeds without an e-stop. If the operator’s hand enters the machine and crosses the light curtain at any other time during the cycle, it will immediately trigger an e-stop. This module can cover up to 2 zones with their own independent mode switching logic. Each zone requires 2 safety devices. Every safety equipment deployment should be paired with a safety assessment to ensure risk reduction.

This document covers requirements for latest version of Vention’s Mode Switching Safety Module. For previous version, refer to link below:

Documentation for Previous Product Versions

Features

  • Compatible with every model of MachineMotion AI

  • Configuration-free, plug-and-play

  • Daisy-chainable

  • For mode switching applications without full body entry

  • Latches faults from Device inputs to MachineMotion AI when mode switching logic is violated

  • 2 independent mode switching zones

  • Compatible with Datalogic SG4 & Keyence GL-R light curtains

  • Compatible with Datalogic & Keyence laser scanners

  • Compatible with fail-safe inductive sensors

  • RGB LED indicator for safety status (emergency stop, faults)

  • Single-color LED indicators for power and communication status

  • Publishes safety state to the MachineMotion AI controller

Included cables

  • 1x Safety Extension cable (5m) - CE-CA-102-5000__3

  • 2x Safety Device Jumper - CE-SA-125-0001

  • 1x Safety Jumper - CE-SA-102-0001

Safety

Vention’s safety modules perform safety functions as a part of a whole installation or machine. A complete safety system normally includes sensors or input units, logic units and contactors or output units. The manufacturer of the installation or machine is responsible for ensuring proper functioning of the whole system. The total concept of the control system into which the safety module is integrated must be validated by the user. Vention cannot guarantee all specifications of an installation or a machine without being responsible for the risk assessment and the design of the safety system. Vention takes over no liability for recommendations which are given or implied in the following description.

The following items must be taken into consideration during the design, risk assessment & installation of the safety system :

  • The Safety Modules shall be put into operation only after the safety functions have been tested during the commissioning.

  • According to EN IEC 60204-1:2018 and EN ISO 10218-1:2011 it is not allowed to restart automatically after emergency stop. Therefore the control systems of the connected devices have to disable the automatic start after emergency stop.

  • Opening the Safety Module or implementing unauthorized changes voids any warranty.

Functional error! Danger to life, risk of serious injuries or property damage

  • The Mode Switching Safety Module AI may only be used in VENTION safety ecosystem;

  • The Mode Switching Safety Module AI does not monitor the input redundant signals at the Device ports. If the connected devices do not have monitoring of its output signals, the performance level of the safety function can be reduced;

  • No emergency stop button shall be connected to the Safety IN port;

  • Mode switching is not designed for full body entry. As there is no latch on the monitoring of the safety device ports 1A and 2A, it is not acceptable to allow full body entry;

  • When using the mode switching function, it shall be ensured that the safety device ports 1B and 2B represent the safe state of the application. As there is no latch on the monitoring of the safety device ports 1B and 2B, these safety inputs shall always be low if the machinery is in an unsafe state or location;

  • The risk assessment shall demonstrate that when triggering the safety devices connected to the Device ports, the state of the machine and the safety distance are acceptable. Refer to ISO 13855 and ISO 13857 for additional considerations on safety distances;

  • The Mode Switching Safety Module AI is designed to operate in indoor environments without dust or high humidity. Dust and dampness may lead to malfunction. Do not install or operate the Safety Module outdoors;

  • The machine shall be designed in such a way that it is not possible to press the reset button from inside a safeguarded area without triggering one of the devices connected to the Device ports.

Technical specs

General Specifications

Item

Specification

Part Number

CE-SA-018-0001__2

Weight

0.8kg

Dimensions

19.0 x 15.0 x 9.0mm

Material

  • Bottom enclosure: Aluminum

  • Top enclosure: Aluminum

Operating Temp

0 to 40°C

IP rating (IEC 60529)

IP54

Electrical Specifications

Item

Specification

Nominal input voltage

24 VDC (Class 2 or SELV power supply)**

Input voltage range

19.2 ~ 26.4 VDC

Operating power consumption

5 W without safety devices

Short circuit protection

Internal electronic fuse, max 2.5A

** Note: In North America, the Safety Module shall be supplied by a certified class 2 power supply. In Europe, the Safety Module must be supplied by an SELV circuit. When powered by the MachineMotion AI those requirements are met.

Physical Interface

Figure 1: Physical Interface

Figure 1: Physical Interface

LED Indicators

Name

LED Color

Indicates (when ON)

POWER

White

Power supplied to the module

COMM

White

Ethernet communication functional

FUSE

Red

Module internal fuse tripped

STATUS

Off

Module disconnected

STATUS

Green

System operational

STATUS

Orange

Error

STATUS

Red

Emergency stop due to upstream module

STATUS

Blinking Red

Emergency stop due to mode switching violation

STATUS

Blinking Blue

Mode switching active

Functionality

In a given zone (Zone 1 or Zone 2), if Device A and Device B are triggered at the same time, the module will trigger and latch a fault on the Safety Out towards the MachineMotion AI controller. The fault is latched until a reset signal is received. The 2 zones’ logic operate independently.

Figure 2: Mode switching logic

Figure 2: Mode switching logic

Port Definitions

Figure 3: Mode Switching Safety Module AI ports

Safety Out - M12, male, 12-pin, A-Keyed

The Safety Out port connects to the Safety In port of the MachineMotion AI, or to another Safety Module when daisychaining.

Pin

Function

Pin 1

24 VDC input

Pin 2

0V input

Pin 3

OSSD output A

Pin 4

24 VDC input

Pin 5

OSSD output B

Pin 6

24 VDC input

Pin 7

Reset input

Pin 8

0V

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

Safety In - M12, female, 12-pin, A-Keyed

The Safety In port connects to the Safety Out port of another Safety Module when daisychaining. If the port is unused, plug the included yellow jumper (CE-SA-102-0001).

Pin

Function

Pin 1

24 VDC output

Pin 2

0V output

Pin 3

OSSD input A

Pin 4

24 VDC output

Pin 5

OSSD input B

Pin 6

24 VDC output

Pin 7

Reset output

Pin 8

0V output

Pin 9

Ethernet RX+

Pin 10

Ethernet RX-

Pin 11

Ethernet TX+

Pin 12

Ethernet TX-

Device 1A/1B & Device 2A/2B - M12, female, 12-pin, A-Keyed

The Device 1A/1B and Device 2A/2B ports connect to safety devices. If any of these ports is unused, plug the included black jumper (CE-SA-125-0001).

Pin

Function

Pin 1

24V (fused)

Pin 2

0V

Pin 3

NC

Pin 4

NC

Pin 5

OSSD input A

Pin 6

NC

Pin 7

NC

Pin 8

OSSD input B

Pin 9

NC

Pin 10

NC

Pin 11

NC

Pin 12

0V

Mounting

Install the module mounting bracket (CE-HW-005-1002) to the extrusion with the screws provided (HW-FN-003-0018). Install the module onto the mounting bracket as illustrated below.

Figure 4: Module Mounting

Figure 4: Module Mounting

Figure 4: Module Mounting

Figure 5: Module Mounting

Wiring Diagram

Figure 6: Mode Switching Safety Module AI wiring diagram

Diagram showing Keyence and Datalogic light curtains with connection details and safety modules.

Figure 7: Mode Switching Safety Module AI wiring diagram with 2x Light Curtains

*Note: Insert a jumper on any unused safety input for proper functionality. See table below to identify the appropriate jumper part number (included with the module).

Jumper Part Number

Description

Target module

Port restrictions

CE-SA-125-0001

M12, male, 12 pins, black jumper

Muting Safety Module AI (CE-SA-015-0001__2)
Mode Switching Module AI (CE-SA-018-0001__2)
Auto-Reset Module AI (CE-SA-019-0001__2)

Strictly reserved for Device ports

CE-JP-000-0002

M12, male, 4 pins, yellow jumper

Access Request Module AI (CE-SA-017-0001__2)

Strictly reserved for End Effector port

CE-SA-102-0001

M12, male, 12 pins, yellow jumper

All modules

Other unused safety input ports

Important information

  • The electronic fuse contained in the Mode Switching Safety Module AI protects from internal faults and external faults, but only on the Device ports. The 24V power output on the Safety In port is not protected by the electronic fuse. The electronic fuse has an auto-retry mechanism (it does not latch faults and does not require a power cycle to reset).

Safety Data

The Vention’s Safety Modules realize the following safety functions :

  • System emergency stop output at the Safety OUT connector from the Safety IN port (E-stop_SafetyIN-to-SafetyOUT);

  • The Device port (light-curtain or area scanner) to the Safety OUT portSystem emergency stop output at the Safety OUT connector from a Safety Device port (E-stop_Device-to-SafetyOUT); and

  • System reset propagation from the Safety IN port to the Safety OUT port (Reset_SafetyOUT).
    For each of these functions, safety data can be found in the following table.

For each of these functions performed by the Robot Safety Module, safety data can be found in the following table:

Safety Function

PL

Cat.

MTTFd

DCavg

PFHd

Response time

E-stop_SafetyIN-to-SafetyOUT

e

3

224

99%

4.29E-08

20 ms

E-stop_Device-to-SafetyOUT

e

3

224

99%

4.29E-08

20 ms

Reset_SafetyOUT

c

1

>100

N/A

1.14E-06

Not Applicable

The above information have been calculated based on the following operation conditions:

Data

Value

Unit

dop

365

days/years

hop

24

hours/days

tcycle

8640

s/cycle

Documentation for Previous Product Versions

Mode Switching Safety Module AI Datasheet